DesignCon 2018 has passed. For those involved from the high-speed communications and semiconductor communities, everyone needs time to catch their breath a bit before planning for the rest of 2018. Why? DesignCon always offers exposure to the latest state-of-the-art design methodologies, applications, technologies, and unparalleled networking opportunities. One question was on the minds of many: How real is 112 Gbps PAM4? The number of demos and presentation at DesignCon prove the … [Read more...]
Search Results for: 112 Gbps PAM4
SI Journal Online Panel: Challenges for 224 Gbps Systems
The need for speed is the relentless driver for every higher data rate system. Each new advance in data rate and signal bandwidth brings with it a new set of challenges in interconnect and I/O transceiver technologies as well as the picks and shovels that enable shorter time to market ever more advanced systems. This panel discussion brings together experts in the industry to present solutions to the most difficult design and system challenges when migrating products from the 56 Gbps or 112 Gbps … [Read more...]
Connectors Address Challenges of 224 Gbps PAM4 Design
Delivering 224 Gbps PAM4 signals will require careful analysis of signal integrity and thermal effects, as well as the development of enabling technologies and new methodologies to achieve clean signals at these data rates. Industry-leading experts are focused on this topic, developing new technologies as well as products to handle high-speed data, and engaging in interoperability demonstrations at tradeshows, demonstrations of new products for 224 Gbps PAM4 systems, and numerous ongoing … [Read more...]
224 Gbps PAM4 Interconnect Solutions
Samtec next-generation interconnect solutions are designed with the flexibility and performance to meet the challenges of 224 Gbps PAM4 architectures. Emerging system requirements are driven by industry advancements in areas such as data centers, artificial intelligence (AI), machine learning (ML), and quantum computing, and Samtec’s products and roadmaps are carefully designed to satisfy these high-performance needs. On-Package or ASIC-Adjacent Cable System OSFP 224 Gbps PAM4 … [Read more...]
New High-Performance 90 GHz Test Solution Enables 224 Gbps PAM4 SerDes Characterization
The demand for bandwidth is pushing the limits of test and measurement to speeds and fidelity not previously possible. Complex systems, such as 5G and 6G networks, high-speed SerDes, automotive radar, artificial intelligence, machine learning, and augmented and virtual reality, require much higher frequencies for evaluation. Even though 112 Gbps PAM4 is just now becoming fully available within the market, 224 Gbps PAM4 SerDes characterization is already knocking at the … [Read more...]
Samtec’s First 224 Gbps PAM4 Live Product Demonstration
There’s no end to the demand for bandwidth. Everything from 5G networks, streaming video, social media, augmented and virtual reality, and artificial intelligence and machine learning, are all pushing current-bandwidth limits. The next level is 224 Gbps PAM4. Visitors at DesignCon 23 saw promises and glimpses of 224 Gbps equipment and components. We are excited that we debuted our first 224 Gbps PAM4 live product demonstration. In this video, Ralph Page, Systems Architect at … [Read more...]
Why Did PCIe 6.0 Adopt PAM4? There Are Many Reasons.
Samtec is a proud member of the PCI-SIG® community, and we have been for many years. In conjunction with our friends at PCI-SIG, Jignesh Shah, Senior System Architect at Samtec, discusses PAM4 encoding, which is a new feature of the PCIe® 6.0 specification. New: The PCIe® 6.0 Specification In early 2022, PCI-SIG® released the full version of the PCI Express® (PCIe®) 6.0 specification. As with previous versions, the latest version doubles the data rate of the PCIe 5.0 specification and … [Read more...]
Samtec at SC22: New Products, Technologies, and 112 Gbps Demos
The global high-performance computing (HPC) ecosystem comes together each year at SuperComputing. SC22 offers data analysts and scientists, system architects, and design engineers the opportunity to learn, network, and explore the latest in HPC solutions. As a global high-performance interconnect solutions provider, Samtec is a long-time sponsor of SuperComputing. This year, Samtec will feature the latest interconnect solutions in real-world high-performance product demonstrations. The … [Read more...]
Overcoming The Challenges of Achieving 224 Gbps Performance
In this video from DesignCon 2022, Keysight's Mike Resso refers to 224 Gbps as a "blindingly fast speed." Ten years from now, when 224 is old-hat and commonplace, we will look back at that statement and smile at how far we've come since those technologically backward, archaic days of 2022. But as of today, achieving that data rate is bleeding-edge and state-of-the-art. This video, with Mike and Samtec's Jignesh Shah, discusses several topics related to 224 Gbps performance, including ... … [Read more...]
Six New 112 G Connector Systems Is The Coolest Demo At DesignCon (IMHO)
This live demonstration from DesignCon 2022 shows six of Samtec's 112 Gbps PAM4 connector systems. It includes board-to-board connector sets, as well as two Samtec Flyover® cable systems. One is a mid-board to cable backplane configuration, and the other is mid-board to front panel. These cable systems are emulating real-world data center system architectures. Each board has four Alphawave AlphaCORE Multi-Standard SerDes. For each connector set, the Alphawave SerDes is transmitting 112 Gbps … [Read more...]
- « Previous Page
- 1
- 2
- 3
- 4
- 5
- 6
- …
- 21
- Next Page »