Gold Plating On Connectors: How Much Do I Need?

Gold Plating -- Gold prices - Mar 2025

Designers frequently ask how much gold plating they should specify on the connector pins. As I write this blog (and yes, I’m old-fashioned and am actually typing it; I’m not using AI), and have updated it in April 2025, the price of gold has increased about 23% since the beginning of the year (currently at about $3,200/ounce). So, the original question – how much gold should I use on my connectors – is extremely relevant.

Gold Plating Is A Major Cost Driver

The major costs in a connector set are:

  • the plastic body
  • the pins
  • the plating on the pins
  • the labor to assemble it
  • and the packaging.

And on most connectors – well, most Samtec connectors anyway – the bigger ticket items are the pins and the plating.

For example, on a micro-pitch, high-density interconnect product, the pins and plating may account for about 25% – 30% of the total cost of the connector. However, on a basic 2.54 mm centerline terminal strip (“header”), it can account for up to 60% – 70% of the total cost of the connector.

.100" Pitch Terminal Strip - gold plating
.100″ Pitch Terminal Strip

That’s because the relative size of the plastic body on a miniature, mold-to-position micro connector is almost always larger than the body on a basic cut-to-position strip-line connector. Conversely, on a basic 2.00 or 2.54 mm pitch strip header and socket, the pins are larger and therefore require more plating.  And, of course, those larger pins are going to cost even more if you’re using gold plating.

So, selecting the right pin and plating significantly impacts the cost of the connector system.

Why Use Gold Plating?

Connector Plating - Tiger Claw C 137 - Gold Plating

Gold is generally specified for high reliability, low voltage, or low current applications. Gold is used in high-cycle applications because it’s rugged and has excellent wear properties (here’s an example of a high-cycle connector). Samtec’s gold is alloyed with cobalt, which increases the hardness. We also recommend gold for hostile environments, because it will remain free of oxides which could cause an increase in contact resistance.

Gold is a noble metal, which means it doesn’t react much to its environment. Also, sometimes gold is a “matter of necessity” in that as connectors shrink in size, the contacts are too small to generate much normal force. So, low normal forces guide the need for Au plating. 

The disadvantages of gold are primarily cost, then porosity at thinner plating levels, and some nuances regarding solderability. Specifically, many customers successfully solder all gold-plated pins to the PCB. But, they are not soldering to the Au, because the Au dissolves in the molten solder. They are soldering to the nickel under the Au. So, technically, it is correct to say Au has poor solderability. 

How Much Gold Plating Do I Need?

The quick answer is to use whatever amount meets your system requirements at the lowest cost. In other words, make sure it works and meets your quality design specifications, but don’t over-design on the plating.

connector plating FAQ Samtec pins on reel in factory

But how much gold is enough? Unfortunately, there’s no answer that we can guarantee is right for every application. But, for simplicity’s sake, we can tell you that the vast majority of Samtec customers who use gold plating can be divided into three categories: 

  • very light gold (about 3 µ”, or “flash”)
  • “standard” gold (10 µ”)
  • and heavy gold (30 µ” or more).

Very light gold, or “flash” gold plating, is used in applications where the connector set will have a relatively easy life, AKA, an office environment. An “easy life” means the mated connector set is:

  • Not going to be cycled, or plugged and unplugged, much. Like maybe 10 – 15 times, depending on the contact selected (1).
  • In a clean environment where it’s not subject to any corrosive chemicals or vapors.
  • Not subject to temperature swings, or higher temperatures, and it’s in a low-humidity setting.   
  • Not subject to shock and vibration, and it won’t be dropped or manhandled.

Conversely, heavy gold is used in applications where the connector set is:

  • Going to be cycled, or plugged and unplugged frequently. This refers to 100 cycles or more, depending on the contact system (1).
  • In a harsh environment where it is subject to high temperature, high humidity, swings in temperature and humidity, and corrosive chemicals or vapors.
  • The application is subject to higher shock and vibration.
  • The equipment’s failure will lead to catastrophic results, like the loss of life or injuries.

It’s interesting that the requirements that would qualify a connector for “standard” gold plating are arguably the most vague. -L plating (usually 10 µ” of gold in the contact area) is the plating option most Samtec customers select. In other words, the majority of Samtec customers use “standard” gold thickness — 10 µ” of gold — and it works just fine in their applications.

BTW, I mention three of our gold plating options above. Many Samtec products are available with a wide variety of plating options, from all tin, to gold flash, to extra heavy gold, to tin/lead, and others.

FYI, years ago, most gold-plated connectors required 30 – 50 µ” of gold, driven by industry standards like Bellcore specs. Rising gold prices in the late 1970s, 1980s, and into the 1990s led to Telecordia specs, which required a connector to meet a performance specification rather than a plating thickness. In my recollection, that’s when the demand for heavy gold began to wane.

It’s Much More Than Just Plating Thickness

If you’re still reading, please stay with me for another minute or two. This is important stuff:

popular connector Rugged, Industrial, Tiger Eye Samtec

(1) First, the plating thickness is not the only factor that determines the success of a mated connector system. It’s essential that the contact system selected meets the demands of the application. Samtec offers several contact systems, on a variety of centerlines and stack heights, depending on your design requirements. For example, a Samtec Tiger Eye™ contact system is designed for high reliability, high cycle applications. It features a multi-finger contact – with either three or four points of contact – made of heat-treated beryllium copper. With the right plating, this contact system has been tested to over 1,000 cycles. Other contact systems, made of lesser metals and with fewer points of contact, will not reach 1,000 cycles even with 50 µ” of gold.  Here’s a link to a blog on this subject if you want to learn more. 

Second, you must take into account other specifications like the normal force of the mated connector set, possible effects of dissimilar metals and galvanic corrosion, underplating and their thicknesses, solderability, the operating temperature of the connector and its impact on performance, voltage and amperage, amount of vibration, and other factors. It’s not just the plating! Here’s a link to a blog that begins to address these and other issues.

Third, if your system requires your connectors to be tested beyond typical industry standards and specifications, many of which are common requirements for harsh environment applications/industries, check out our Severe Environment Testing (SET) initiative.

Driven by demands for high-functioning commercial standard interconnects, SET has proven beneficial in providing performance confidence, not only for rugged Mil/Aero industries and applications, but also for Automotive, Industrial, and Medical applications.

And, if your application requires very high mating cycles, Samtec ELP products are tested to rigorous standards that evaluate contact resistance in simulated storage and field conditions. These connectors have passed a nasty 10-year Mixed Flowing Gas (MFG) test, are tested to very high-mating cycles (250 to 2,500), and a variety of connector types and pitches available.

And finally, we’re here to help. If you have questions about any Samtec connector product, application, or plating, contact the Application Support Group.  

You May Also Enjoy:

Leave a Reply

Your email address will not be published. Required fields are marked *