The Science of Optical Interconnects, Part 1

Why Copper Is Running Out of Road

The history of electronics is full of predictions that turned out to be wrong. One of my favorites dates back to the early days of structured networking. Around thirty years ago, I attended a training course on premises wiring. At the time, 100 Mbps Ethernet was considered cutting-edge technology, and the industry was only just beginning to embrace Category 5 cabling. During the course, an industry expert confidently declared that copper had reached its practical limit. Future networks, we were told, would inevitably rely on fiber optics. Yet three decades later, copper is still everywhere.

Optical interconnects and bundles of fibers offer space, weight and thermal advantages over copper cables.
Bundles of fibers offer future-proof performance

Not only has copper survived, but it has thrived. Connector manufacturers now routinely support data rates that would have seemed impossible at the time. Technologies such as PAM4 signaling, advanced equalization, precision connector design, and low-loss cable systems have repeatedly extended the useful life of electrical interconnects far beyond what many experts expected.

Betting Against Copper

History suggests that betting against copper is usually a mistake, but something interesting is happening.

For much of the modern computing era, increasing performance was largely a semiconductor problem. Faster processors and denser memory devices drove successive generations of system performance. Connectors evolved alongside the silicon, but rarely attracted the same attention.

As artificial intelligence, cloud computing, and high-performance computing continue to expand, system architects are discovering that moving data is becoming almost as challenging as processing it. The interconnect is becoming one of the defining factors in overall system performance, rather than simply the plumbing that joins together more important components.

This helps explain why a technology many engineers still regard as specialist is suddenly appearing in conversations throughout the industry. Fiber optics are hardly new, but the factors that once made copper the obvious choice are being challenged in ways that were difficult to imagine even a decade ago.

Before we explore how optical fiber works, it is worth understanding why the industry is starting to look beyond conventional electrical signaling.

Copper Has Been Here Before

The first thing to understand is that copper is remarkably resilient. Every generation of high-speed design has introduced new challenges: signal loss increases as frequencies rise, and crosstalk becomes more difficult to manage. To counter these and many other effects, connector geometry has become increasingly important. The industry has responded with a range of innovations aimed at preserving signal integrity at ever-higher data rates.

New materials, improved simulation tools, better connector designs, more sophisticated encoding schemes, and advances in signal conditioning have all helped push copper performance further than many thought possible. The connector industry has become exceptionally good at solving these problems.

That success is one reason why engineers often remain skeptical when they hear claims that fiber optics will replace copper. But the question is not whether copper works – clearly it does. Rather, the question is whether it remains the most efficient solution as system requirements continue to grow.

The Rules Are Changing

Traditionally, communication channels were designed to carry data between devices. Today, they are increasingly being asked to support entire computing fabrics.

Modern AI systems provide a good example. Training clusters may contain thousands of accelerators working together on a single workload. Information must move continuously between processors, memory resources, and storage systems. The volume of data being exchanged is extraordinary.

Bandwidth is no longer simply a specification on a datasheet. It has become an architectural requirement. System designers must balance bandwidth, latency, power consumption, and physical density simultaneously, and improving one often affects the others.

Every electrical channel introduces loss, distortion, and other effects that degrade signal quality. As frequencies increase, maintaining signal quality requires increasing amounts of engineering effort. Active techniques such as equalization, retiming, and signal conditioning all help preserve data integrity. Many are highly effective, but they also consume power and add complexity, especially as modern data rates rise. A growing proportion of system resources are spent overcoming the limitations of the communication channel itself.

When Bandwidth Becomes an Architectural Problem

Alongside power consumption, physical density is equally important.

In copper technologies, increasing bandwidth often means adding more connections. Modern systems continue to achieve higher performance in much the same way, but AI workloads have pushed this approach to a dramatically different scale. Every new connection requires routing space and consumes power. With power consumption comes heat, and thermal management has a real impact on connector design.

A modern switch or accelerator may need to support extraordinary levels of connectivity while operating within strict power and thermal limits. Designers must consider how much data can be moved per watt, per rack, and per square centimeter of package area.

This is one of the reasons why concepts such as co-packaged optics, silicon photonics, and optical interconnect fabrics are attracting so much attention. They are not simply new products. They represent attempts to address system-level challenges that become increasingly difficult to solve using electrical signaling alone.

None of this means that copper is failing. Rather, it means that engineers are increasingly being asked to make informed choices about where copper makes sense, where optics offer advantages, and how the two technologies can work together.

Looking Beyond Copper

It is tempting to think of fiber optics and copper as competing technologies, but the relationship is far more collaborative than competitive.

Copper is still highly effective. It remains the only realistic choice for most power delivery applications, and it is still suitable for many short-reach communication links. It is familiar, robust, cost-effective, and supported by decades of engineering expertise. There are countless applications where copper is still the best solution available, and so the growing interest in optics is driven by the recognition that different communication media excel at different tasks.

Engineers have always selected technologies based on the problem they are trying to solve. As bandwidth demands continue to increase, and as system architects search for more efficient ways to move information, optical technologies are becoming increasingly attractive. But fiber optics still feel unfamiliar. Electrical systems are intuitive. Contacts touch, current is transferred and signals move. Light seems to behave differently.

Fiber optics are not nearly as mysterious as they first appear. They are just another way of transporting information from one place to another. The underlying physics may be different, but many of the engineering principles are familiar.

In the next article of this series, we will take a closer look at how optical fiber actually works. We will explore how light can be guided through a strand of glass thinner than a human hair and discover why a technology that some engineers still approach with caution has become one of the most important communication media in the modern world.

If you can’t wait for the next installment, visit the Samtec website to find out more about our fiber technology.

You May Also Enjoy:

Leave a Reply

Your email address will not be published. Required fields are marked *