Check out the new Samtec Optical Group video. The Samtec Optical Group is an engineering team dedicated to the design, development and application support of high performance micro optical engines, active optical assemblies and high density ganged passive optical panel solutions. Capable of 14 Gbps, 28 Gbps, and soon 56 Gbps, Samtec’s FireFly™ micro on-board optical engines occupy the smallest overall footprint, consume the least amount of power, and enable fast, easy, and low cost fiber … [Read more...]
Search Results for: firefly
A Look Inside Samtec’s High Speed Cable Tech Center
Check out the new Samtec Cable Group Tech Center video. It’s an overview of the Samtec Cable Group, our R&D and manufacturing Technology Center focusing on precision extruded micro coax and twinax cable used for high speed / high density cable assemblies, including 26-38 AWG, 50/75/85/100 ohm impedance, and systems rated at 28+ Gbps. Cable Options Samtec Cable Group offers a variety of center conductor, dielectric, shielding, and jacket options. Center conductor options include … [Read more...]
Samtec and Amphenol® Aerospace Partner to Address the Growing Need for Rugged Optics
Samtec and Amphenol® Aerospace recently announced a partnership to incorporate Samtec’s FireFly™ optical cable platform with Amphenol® Aerospace’s bulkhead interconnects for rugged optic solutions. Click here to read the official press release. FireFly™ Samtec’s FireFly™ is a mid-board cable and optical interconnect system. FireFly™ is incredibly dense, and it enables chip-to-chip, board-to-board, and system-to-board connectivity using the same connector system for both copper … [Read more...]
Get the Target for the Next Generation “Samtec Reality” App
Click the Target Above to Print The next generation of the Samtec Reality app combines all the great features of our existing virtual product sample experiences – Augmented Reality and Virtual Product Explorer – into one amazing “super app” designed to provide an even more in-depth, user-friendly way to explore our latest technologies and products. How to Use the AR Feature: Click on the target image to download and print Click here to download the app from the App Store Open the … [Read more...]
Come to See Samtec At New Tech, Israel
Please visit Samtec at the New Tech Exhibition - 2015, on 19 and 20 of May. We are at booth #40. You can see several of our major new products, including: ExaMAX® backplane systemsZ-Ray™ high density, low profile interposersAdditions to the SEARAY™ line of high density, open-pin field arraysFireFly™ future-proof, Micro Flyover™ system The New–Tech 2015 Exhibition is the largest and major exhibition of the Hi–Tech & Electronics in Israel. More than 140 companies, who lead these … [Read more...]
Samtec Joins IRT Nanoelec Silicon Photonics Program
Samtec is pleased to announce its entrance in the Silicon Photonics Program of the IRT Nanoelec headed by CEA-Leti. Samtec is joining CNRS, STMicroelectronics, Mentor Graphics and CEA-Leti to develop and industrialize optical communications solutions using Silicon Photonics technology for addressing Data Centers and High Performance Computing applications. Officials from all parties expressed their enthusiasm. “We are thrilled with the opportunity to join the Silicon Photonics Program of the … [Read more...]
Be Sure to Visit Samtec at OFC
We hope you can visit us at OFC, March 24-26, at the Los Angeles Convention Center. Our booth (#1849) will have two high-speed product demonstrations and onsite experts to bring you up-to-speed about several new Samtec products. Our physical product demonstrations include a FireFly™ 12 channel optical Micro Flyover™ System operating at 28 Gbps/channel (336 Gbps aggregate), and Samtec ExaMAX® backplane systems at 28 Gbps/channel (1 Tbps/connector pair) and 40 Gbps/channel (1.25 Tbps/connector … [Read more...]
Papers, Product Demos, New Products At DesignCon 2015
Samtec, Inc., and Teraspeed® Consulting are presenting five technical papers, giving two physical high speed product demonstrations, and showcasing several new products at DesignCon 2015. Samtec’s new location is booth #943, and Teraspeed® Consulting is booth #1048. Samtec’s presentations are: Optimizing Symmetry in Open Pin Field Designs – Wednesday, January 28 – 2:50pm – 3:30pmCausality Demystified – Thursday, January 29 – 8:30am – 9:10am Teraspeed® Consulting’s presentations … [Read more...]
Julian Ferry Interview On High Speed Interconnect Design Developments
Julian Ferry, Samtec’s High Speed R&D Manager, recently spoke to Connector Supplier about the latest developments in high speed interconnects, the applications driving them, and how Samtec is meeting the challenges. Here is a full copy of the interview, courtesy of Connector Supplier. Q&A: Samtec on Signal Integrity. By Patricia Staino, June 16, 2014 Recently we spoke to Julian Ferry, high-speed R&D manager at Samtec, to learn more about the latest developments in high-speed … [Read more...]
Micro Flyover Cable System Allows Future-Proof Designs
Samtec's FireFly™ Micro Flyover System is an inside-the-box interconnect system that gives designers the option to future-proof their systems. This future proofing allows an easy upgrade from copper to optical with the same connector and footprint. With the highest 14 Gbps bandwidth density available, the FireFly™ system enables chip-to-chip, board-to-board and system-to-system connectivity at data rates up to 28Gb/s (in development). By taking the data connections “off-board” with flyover … [Read more...]
- « Previous Page
- 1
- …
- 23
- 24
- 25