Signal Integrity expert Eric Bogatin recently shared three predictions on the state of signal integrity. Based on his discussions at DesignCon 2016 and thereafter, Eric has three predictions about major changes ahead for high speed serial link systems. The first is the rollout of 28 Gbps systems will be slower than expected. Eric explains that the semiconductor companies producing the CMOS devices – ASIC, FPGA or custom – are doing fine producing the silicon with acceptable performance at 28 … [Read more...]
Search Results for: firefly
Samtec Releases Twinax Flyover Application Design Guide
The march to faster data rates never seems to stop. Communications protocols used in the data center provide the proof. Fiber Channel signals can run up to 32 Gbps. 25G Ethernet 802.3bj and Ethernet 100G signals can run up to 25Gbps. InfiniBand EDR 104G serial channels support 26 Gbps data rates. This presents engineers of high-speed serial channels with a number of PCB design challenges. Some of the key limitations of PCBs running at 28+ Gbps include trace … [Read more...]
Samtec Updates Broadcast Video Solution Guide
Streaming HD video and 4K/8K UHDTV are just two examples of a continuing evolution in video signaling. Video has transformed from being an analog 6 MHz bandwidth signal to a 12 Gbps digital data stream. As signaling has transitioned into the digital domain, first in SD and HD formats, and recently at 6 Gbps and 12 Gbps 4K UHD-SDI standards, the demand for meeting stringent return loss requirements up to 12 GHz has emerged. Samtec offers a full line of high-speed board-to-board and RF … [Read more...]
High Speed Signal Transfer Rates At 28 Gbps (OFC 2016)
In this video, Kevin Burt, of the Samtec Optical Group, discusses another demonstration from OFC 2016. This is a system level demonstration of high speed signal transfer rates at 28Gbps, FireFly™ high speed optical links at 28 Gbps, and signal quality performance of ExaMAX® backplane connector. Kevin discusses the advantages of the industry's first Flyover QSFP28 (FQSFP) System. This approach removes signals from their traditional pathways—copper traces … [Read more...]
14 Gbps Optical Link In FMC VITA 57.1 Form Factor For FPGA Applications (OFC 2016)
Kevin Burt, of the Samtec Optical Group, discusses one of two demonstrations at OFC 2016. This is a demo of a FireFly™ 14 Gbps optical link in a FMC VITA 57.1 form factor for FPGA applications, for the high performance computing, rugged military, and industrial markets, to name a few. This demo is an optical interconnection between two FPGAs, with a Xilinx Development Card and two FMCs (FPGA mezzanine cards), one from TechWay and the other from Crossfield Technology. This is 8 lanes of 14 … [Read more...]
Samtec Exhibits at 2016 NAB Show in Las Vegas
One of the biggest tradeshows in entertainment and media is NAB Show. It is the world’s largest annual conference and expo for professionals who create, manage, and distribute entertainment across all platforms At this year’s event in Las Vegas, Samtec will feature a variety of interconnect solutions targeted at the broadcast video market. These include mid-board and panel mount optical systems based on FireFly™ , True75TM 75Ω RF Systems, full turnkey RF cable assemblies, and … [Read more...]
Samtec Expands Optical Product Portfolio
Readers of the Samtec blog know how excited we get talking about our FireFly™ Micro Flyover System™ and the optical engine technology included in FireFly. Sometimes we forget to talk about our other optical products. In recent weeks, Samtec has added to our repertoire of optical product offerings via some product line extensions and new releases. These include the following three product families: PCIEO-4G3, FOPC and OPA. PCIEO-4G3 Option for Active Optical Cable … [Read more...]
Samtec Exhibits at OFC ’16 in Anaheim, CA
One of the biggest tradeshows in the optical world is OFC. At this year’s event in Anaheim, Samtec will be exhibiting a variety of mid-board and panel-mount optical systems. Samtec’s optical and signal integrity expertise enables systems designs with maximum density, minimal cost and performance optimization, while offering a path to 56 Gbps and beyond. Of several products being featured at OFC this year, the FireFly™ Micro FlyOver System™, which enables chip-to-chip, … [Read more...]
OFC Show
OFC is the largest global conference and exhibition for optical communications and networking professionals. OFC offers key networking and partnering opportunities, and provides insights and inspiration on the major trends and technology advances affecting the industry. Visit Samtec at OFC at booth # 2367 to see a system level demonstration of high speed signal transfer rates at 28Gbps, FireFly™ high speed optical links at 28 Gbps, and signal quality performance of ExaMAX® backplane … [Read more...]
Chip-to-Chip at 25 Gbps+ . . . Over Fiber?
As another year dawns, the demand for data remains insatiable. The number crunching of Big Data requires larger and faster supercomputers to analyze immeasurable data sets. New server architectures leverage hardware accelerators – in FPGAs or via expansion cards – to offload system processing. The growth of the IoT gives rise to data acquisition systems aggregating GBs of data. High-speed test and measurement equipment emulate signal traffic found in next generation routers, switches and … [Read more...]