Communication. There are hundreds of books about the various types, styles and strategies. You can earn degrees in the study of it. It’s a life skill everyone must learn, and there is a constant pursuit for ways to more effectively communicate. The PCI Express® standard can help with effective communication, but just for electronic devices instead of people - you'll still need to buy that book. This standard creates a connection for high bandwidth communication between a PCI Express® device … [Read more...]
Samtec and Techway Discuss 25 Gbps Embedded Optical Solutions
Embedded computing solutions are increasing in functionality, density and performance. Fast growing applications range from 5G and ATE to Machine Vision and Edge Computing. High-speed optical communications offer faster throughput and scalability, yet many system architects and hardware engineers are hesitant to move to the optical domain. Embedded Optical Solutions Several solutions on the market help simplify designing in the optical domain. For example, the Samtec … [Read more...]
Samtec Releases New FireFly™ Video
We talk about FireFly™ a lot around here, and why not? With the industry’s leading miniature footprint enabling maximum signal density and SI over longer distances, we assume you want to hear about it. FireFly™ Micro Flyover System™ provides high-performance versatility by taking the data connection “off board” for higher data rates up to 28 Gbps per lane with a path to 112 Gbps PAM4. In addition, the miniature footprint allows for higher density and closer proximity to the IC. The results … [Read more...]
2018 IEEE Avionics and Vehicle Fiber-Optics and Photonics Conference (AVFOP)
The aerospace & vetronics industries have made great strides in recent years deploying fiber optics and photonics technology on commercial and military platforms. This trend will continue to grow as avionics & vetronics fiber optic system architectures, networking schemes, and components evolve and mature. This application-oriented conference will provide an international forum for leaders, researchers, engineers, and manufacturers to convene and discuss issues of deploying … [Read more...]
FireFly™ Finds a Home in PCIe Expansion Cards
PCI Express continues to grow as the de facto I/O expansion bus in a number of embedded computing applications. The flexibility of the PCIe interface and the data rates it supports have spawned a number of standard PCB form factors adopted in many different applications. A common functionality added to many PCIe form factor expansion cards is optical networking. While industry standard active optical cables target typical datacom and telecom applications, a variety of high-speed I/O … [Read more...]
Samtec Exhibits at OFC ’16 in Anaheim, CA
One of the biggest tradeshows in the optical world is OFC. At this year’s event in Anaheim, Samtec will be exhibiting a variety of mid-board and panel-mount optical systems. Samtec’s optical and signal integrity expertise enables systems designs with maximum density, minimal cost and performance optimization, while offering a path to 56 Gbps and beyond. Of several products being featured at OFC this year, the FireFly™ Micro FlyOver System™, which enables chip-to-chip, … [Read more...]
Strike Up The Bandwidth Beyond 28 Gbps
Here is a link to an EDN article you need to read. Scott McMorrow, R&D Consultant for Teraspeed® Consulting (a division of Samtec), discusses the migration of high-speed data transfer rates to 28 Gbps and beyond. Here's a quick synopsis. We Can Barely Get To 56 Gbps With Today's Materials It’s hard to give an overview to such an insightful article, but I’ll try to give a quick recap: First, although many in the industry are successfully achieving information transfer rates … [Read more...]