Design and Processing Engineers frequently contact our Interconnect Processing Group (IPG) to discuss multiple connector alignment issues on mating PCBs. Our standard response is “it’s easy, don't worry about the alignment, and we recommend you use as many mated connector sets as possible.” OK, I’m lying. The first part – that IPG receives a lot of inquiries – is true. The second part – it’s easy – is not 100% true. At times it can be complicated. When using multiple connectors per board, … [Read more...]
Search Results for: searay
Real World 28 Gbps Connector Demonstration
The 28 Gbps Product Demonstrator is an active system that showcases Samtec interconnect products at 28 Gbps and beyond. In this brief video overview, Scott McMorrow, Samtec's CTO of Signal Integrity Products, and Brian Vicich, VP of Engineering, explain that it was designed to showcase Samtec’s products, along with the engineering capabilities of Samtec’s Teraspeed Consulting Group, Active System Group, and the Signal Integrity Group. Real World 28 Gbps The 28 Gbps Product … [Read more...]
Samtec Interconnects In Military, Aerospace
Interconnects for the military/aerospace industry are used in a variety of applications, including communication and navigation equipment, radar, airborne, marine and space guidance control, and electronic warfare, to name a few. While Samtec products are used in commercial applications like the industrial, datacom, telecom, computer and peripheral, instrumentation, medical, and automotive industries, aerospace and military account for a significant portion of our total sales. This is … [Read more...]
Samtec Releases High-Speed Board-to-Board Application Design Guide
If connector speed is a driver of industry growth, then Samtec is leading the pack. We offer not only the largest variety of high-speed board-to-board connectors, but we combine that with full engineering support, online tools and an unmatched service attitude to provide customers with a complete high-speed solution. To support this product line, a new High-Speed Board-to-Board Application Design Guide has been released. This brochure is a great overview of all that Samtec offers in … [Read more...]
12G SDI Signal Processing and Transmission Demonstration (NAB 2017)
Chris Shelly, Samtec's RF/SI Modeling Engineer, walks us through another 12G SDI product demonstration from NAB 2017. This demonstration showcases the Samtec BNC Edge Mount connector used in the Fidus® Gearbox+™ and the Phabrix® QX UHDTV 12G SDI generator/analyzer. This demonstration not only showcases the signal processing capabilities of both of these products, it also highlights the transmission of those signals through several other Samtec 75 ohm PCB connectors. Chris walks us … [Read more...]
Samtec 12G SDI Connectors Performance Demonstration at NAB 2017
Chris Shelly, Samtec's RF/SI Modeling Engineer, walks us through one of two 12G SDI live demonstrations at NAB 2017. This product demonstration showcases live Return Loss testing of different connectors series per the SMPTE ST-2082-1 12G SDI single channel 4K /UHD requirements. The demonstration highlights the custom launch design that successfully allow even the more challenging right angle connector configurations to perform at this high level. With PCB terminated RF … [Read more...]
Samtec 12G SDI At NAB 2017
The North American Broadcast Show, or NAB, is April 22-27 at the Las Vegas Convention Center. NAB is about everything digital in the fields of media, entertainment, and technology. Samtec is exhibiting its line of 12G SDI RF interconnects, including a product demonstration showing live return loss testing of different 12G SDI products, as well as displays of other high-speed interconnects used in the broadcast video industry. If you're in Vegas, we'd love to see you at booth … [Read more...]
Samtec Flyover QSFP In Xilinx VCU118 (OFC 2017)
Kevin Burt, of the Samtec Optical Group, explains another one of the several demos that Samtec presented at OFC 2017. In this demo, four GT 28 Gbps transceiver signals are generated by an FPGA and launched mid-board from a FireFly™ 28 G x4 optical connector system. These 28 Gbps signals then “flyover” the board through a FQSFP twinax cable assembly, to the port, and loop back over the same path, where they are received by the FPGA. The Flyover™ QSFP28 … [Read more...]
Samtec Launches New VITA 57.4 FMC+ ChalkTalk
It seems FPGAs are getting bigger and faster all the time. FPGA vendors continue to integrate more transceivers running at higher speeds in their newest ICs. As an example, the Xilinx Virtex UltraScale+ VU13P FPGA contains 128 GTY transceivers running data rates up to 32.75 Gbps. The increase in number and speed of transceivers on the FPGAs complements the Samtec roadmap of next-generation high-speed board-to-board connectors. Late last year, Samtec announced the … [Read more...]
Samtec Releases New 2017 Full Line Catalog
Every year Samtec releases a new catalog showcasing our full line of products. The latest F-217 Full Line Catalog features new products and technology that enable us to provide overall system optimization from Silicon-to-Silicon. The combination of Samtec’s ultra fast, ultra dense and ultra micro solutions help to streamline the entire signal transmission path from the bare die to an interface 100 meters away and all interconnect points in between. The 2017 Catalog details products … [Read more...]
- « Previous Page
- 1
- …
- 8
- 9
- 10
- 11
- 12
- 13
- Next Page »