Virtual. In a word, that sums up many of our everyday experiences. Gradually, virtual events were popping up. In the tech industry, virtual conferences and trade shows are the "New Normal." One advantage of virtual, or digital, events seems to be popping up. Many in-person tech conferences were cost-prohibitive except for sponsors and key attendees. Virtual events democratize valuable technical content to anyone interested. Does that mean everyone virtual event is of use or beneficial? … [Read more...]
Keysight Quickens Samtec 112 Gbps PAM4 Test and Development Time
Quicken design cycles. Shorter test times. Faster time to market. System architects, product designers and testing engineers have no doubt heard these mantras with every new project they start. Maybe they have had nightmares about these phrases as well! In any case, shorter design and test times and faster time to market are necessary in today's uber-competitive world. Samtec's product development team lives and breathes these mantras everyday. Thankfully, partners like Keysight help … [Read more...]
Optical Data Interconnect (ODI) Ecosystem Solutions Continues to Expand
Next-gen, high-performance Test and Measurement platforms support faster data rates than current solutions. Prevailing devices communicate over copper interfaces in standard form factors and traditional bench instrument applications. At increased data rates, signal integrity concerns over copper cable assemblies and connectors limit the reach and interoperability of systems. The new Optical Data Interface (ODI) is a new high-speed interface standard for advanced instrumentation and embedded … [Read more...]
Avnet XRF16™ Features Samtec Interconnect for 5G Applications
The roll-out of 5G continues despite COVID-19. 5G system development moves on for any number of applications. These include Test and Measurement, Remote Radio Heads (RRHs) and Active Antenna Systems (AAS), Network Equipment and more. The demand for data means design engineers need to quicken time to market. Modular system design provides peace of mind and commonalities from development to production for design-intensive 5G applications. Avnet XRF16™ RFSoC System-on-Module The … [Read more...]
Samtec to Exhibit at OCP Virtual Summit
The global coronavirus pandemic continues to spread. Thankfully, parts of normal life are returning. Employees are slowly going back to work. State parks are opening. Sports leagues like the Budesliga and the NFL are ramping up activities. Light is (finally?) at the end of the COVID-19 tunnel. However, new "normals" may be regular "normals". Trade shows have been "normal" to business. Will they continue to be so? Some of us hope so. In the mean time, many large trade show events have … [Read more...]
Samtec, Mouser and Electronic Design Partner on New 5G Webinar
5G is coming! 5G is coming! Is 5G coming? The first two phrases literally described the global 5G rollout at the beginning of 2020. Handset manufacturers, equipment providers, mobile carriers and industry analysts anticipated a strong year. Is 5G still coming? Well, that depends. Like all parts of life, the 5G rollout has been upended by the unfortunate coronavirus pandemic. Sadly, conspiracy theories linking the virus to mobile towers led to acts of arson. Despite the … [Read more...]
Salt Fog Resistant Optical Modules For Mil/Aero
Data centers drive volume use for modern optical transceivers. These have favorable conditions for the optics, with low humidity and tightly controlled temperatures, which in turn has enabled a low-cost design approach for the subcomponents used in modern devices. The Mil/Aero market has very different environmental requirements with aggressive conditions such as sand/dust, salt fog, and even continuous operation in 100% humidity. These conditions have historically led to the use of robust, … [Read more...]
Samtec Launches gEEk® spEEk Webinar Series
Given the COVID-19 pandemic crisis, it appears the WFH “trend” may become permanent. Indirectly, or maybe directly, the present situation has provided us with yet another way to engage with design engineers and SI experts globally. At home, video streaming is growing exponentially. Professionally, webinars abound on many topics. So, without further ado . . . Samtec is pleased to launch gEEk® spEEk! What is gEEk® spEEk? DesignCon attendees typically look forward every year to … [Read more...]
Samtec Releases Two New Chalk Talk Webinars
Telecommuting. Mobile work. Remote work. Flexible work. Work from home (WFH). They all mean the same thing. What do all of these have to do with Chalk Talks? Who would have guessed so many would WFH? The global COVID-19 outbreak is the reason. So, staying connected is a must. The demand for data hasn't stopped, yet. That requires continued investment both on the edge and in the data center. More data means more speed. How is Samtec responding? With new Chalk Talks, of course! 0 to … [Read more...]
Standards Update: QSFP-DD800 MSA and VITA 57.X
What do the QSFP-DD800 MSA and VITA 57 have in common? Fair question. One focuses on defining the next-gen pluggable form factors while the other complements FPGA mezzanine applications. So what is the link? Samtec, of course! Samtec participates in many Industry Standards to develop commonality is specific applications. QSFP-DD800 and VITA 57 are but two examples. QSFP-DD800 MSA: New HW Spec QSFP28. QSFP-DD. QSFP-DD800. It seems the Multi Source Agreements (MSAs) for Quad Small … [Read more...]
- « Previous Page
- 1
- …
- 14
- 15
- 16
- 17
- 18
- …
- 40
- Next Page »