Regular readers of the Samtec blog are keenly aware of VITA 57 FMC and FMC+ solutions Samtec offers. For more than 10 years, this standard has defined the interface between FPGAs and various expansion modules in a growing number of applications. As FMC/FMC+ leverages open platforms and standards, developers are working to further the adaptation of FPGA technologies in applications ranging from datacom/telecom and broadcast video to instrumentation, aerospace and defense. More and more … [Read more...]
Search Results for: hpc
DesignCon 2018 Parting Thoughts – How real is 112 Gbps PAM4?
DesignCon 2018 has passed. For those involved from the high-speed communications and semiconductor communities, everyone needs time to catch their breath a bit before planning for the rest of 2018. Why? DesignCon always offers exposure to the latest state-of-the-art design methodologies, applications, technologies, and unparalleled networking opportunities. One question was on the minds of many: How real is 112 Gbps PAM4? The number of demos and presentation at DesignCon prove the … [Read more...]
OCP 2018
The 2018 Open Compute Project (OCP) US Summit will be held March 20 - 21 at the San Jose Convention Center. The annual Summit brings together more than 3,000 key decision makers, executives, engineers, developers and suppliers. Together, they help grow, drive and support the open hardware ecosystem in, near and around the data center and beyond. Features of the show include: Keynote presentations by industry titans In-depth discoveries from the Data Center, Networking, Server, … [Read more...]
Samtec New Products At DesignCon 2018
Samtec will be introducing several new products at DesignCon 2018. All of these products are designed to increase data rates, increase system density, and shrink product footprints, so designers can meet their system signal integrity needs. NovaRay™ High Bandwidth, High Density Array Samtec’s NovaRay™ is an industry-leading high bandwidth, high-density interconnect system. The pin-to-ground differential pair configuration enables very low crosstalk to 40 GHz+, tight impedance … [Read more...]
VITA 57 Solutions Enable Scalable ASIC Development Platforms
Readers of the Samtec blog know that FPGAs offer the most flexible electronics development platform in the world. Diverse applications ranging from machine learning and embedded vision to 5G wireless and cloud computing leverage the configurability and programmability of FPGAs to scale I/O, computing and DSP functionality. FPGAs are also frequently used in next-generation ASIC development projects. FPGAs allow for fast and accurate ASIC modeling and verification with accelerated … [Read more...]
DesignCon 2018
Samtec high-speed technologies for Silicon-to-Silicon optimization will be on display, including demonstrations of our state-of-the-art Product Demonstrator featuring several new products: NovaRay™, AcceleRate® HD, and Flyover QSFP28 to Direct Pluggable cable assembly. Other spotlight products include ExaMAX® 56 Gbps PAM4 backplane system, Flyover QSFP28 double-density cable assembly, and AcceleRate® 56 Gbps NRZ slim body cable system. Samtec is in booth #841. About Samtec | Featured … [Read more...]
New FPGA Development Platforms Feature Samtec High-Speed Solutions
FPGA system designers have no shortage of FPGA options for their next-gen end market solution. Xilinx continues to expand their UltraScale+ families. Intel PSG/Altera will ramp Arria 10 and Stratix 10 solutions well in to 2018. New FPGA products require a new generation of FPGA development platforms. Thankfully, both the Xilinx and Intel PSG/Altera design partner ecosystems thrive at launching just what the market needs. Several new platforms feature key Samtec interconnect options that … [Read more...]
Daily Updates from SuperComputing 2017 – November 15, 2017
SuperComputing 2017 remains in full force this week from the Colorado Convention Center in Denver. There are lots of activity in presentations, seminars, demonstrations and exhibits on the tradeshow floor. Stay tuned to the Samtec blog the rest of the week for more highlight. CCIX Interconnect Standard FPGA acceleration of high-performance algorithms remains a constant and growing theme in the supercomputing industry and at SC17. Several new approaches to improve the flow of data … [Read more...]
Daily Updates from SuperComputing 2017 – November 14, 2017
The high-performance computing (HPC) industry is converging in Denver this week for SuperComputing 2017. Representatives from universities, hardware providers, system designers, cloud services, semiconductor and interconnect suppliers (Samtec!) and other participants are sharing ideas and launching new products at this annual event. Samtec's team of technical experts are roaming the convention floor, attending classes and visiting with partners and customers. Stay tuned to our blog this … [Read more...]
28 Gbps Of Data Over Six Feet Of Copper Cable
28 Gbps Steve Leibson(1) and our friends at Xilinx® recently posted a blog about an interconnect system that carries four lanes of 28 Gbps data over six feet of cable. Since this is a Samtec blog, of course it's a Samtec connector they're talking about. The Xilinx blog references a short video that shows a Samtec QSFP28 copper flyover™ carrying four lanes of 28 Gbps serial data error free over six feet of copper twinax cable with plenty of margin. Steve goes on to point out that … [Read more...]
- « Previous Page
- 1
- …
- 8
- 9
- 10
- 11
- 12
- Next Page »