Samtec has been analyzing launch design optimization techniques to improve signal integrity in high frequency test applications for many years, and continues to build upon initial findings for 224 Gbps test systems. In this blog, Part 1 of the series "How to Improve Signal Integrity for 224 Gbps Test Systems," we'll be examining a few key principles for improving signal integrity from the test instrument to the device under test (DUT). These principles are outlined in Samtec's recent published … [Read more...]
Search Results for: 224 Gbps
New 224 Gbps PAM4 Interconnect Solutions With Impressive Performance
Samtec next-generation connector solutions are designed to meet the challenges of 224 Gbps PAM4 architectures. At DesignCon 2024, Samtec had five product demonstrations and displays showcasing our 224 Gbps products. Many incorporated Si-Fly HD™, our new chip adjacent (or on-package) Samtec Flyover® Cable system. In the video above, Jonathan Sprigler, High-Speed Product Manager at Samtec, walks you through some of the 224 Gbps demos and displays in the Samtec booth. First, Jonathan … [Read more...]
SI Journal Online Panel: Challenges for 224 Gbps Systems
The need for speed is the relentless driver for every higher data rate system. Each new advance in data rate and signal bandwidth brings with it a new set of challenges in interconnect and I/O transceiver technologies as well as the picks and shovels that enable shorter time to market ever more advanced systems. This panel discussion brings together experts in the industry to present solutions to the most difficult design and system challenges when migrating products from the 56 Gbps or 112 Gbps … [Read more...]
Connectors Address Challenges of 224 Gbps PAM4 Design
Delivering 224 Gbps PAM4 signals will require careful analysis of signal integrity and thermal effects, as well as the development of enabling technologies and new methodologies to achieve clean signals at these data rates. Industry-leading experts are focused on this topic, developing new technologies as well as products to handle high-speed data, and engaging in interoperability demonstrations at tradeshows, demonstrations of new products for 224 Gbps PAM4 systems, and numerous ongoing … [Read more...]
Samtec Supports 224 Gbps at DesignCon 2024
Are you headed to DesignCon 2024? If yes, be sure to stop by the Samtec Booth (#939) to see demonstrations of products that address interconnect needs all the way up to 224 Gbps. New and established Samtec products on display will include those used in front-panel, mid-board, and backplane applications, including our new backplane solutions, optical mid-board options, and test point system. Look for our green shirts at the Welcome Reception on Tuesday and say hello! Try to make some time to … [Read more...]
224 Gbps PAM4 Interconnect Solutions
Samtec next-generation interconnect solutions are designed with the flexibility and performance to meet the challenges of 224 Gbps PAM4 architectures. Emerging system requirements are driven by industry advancements in areas such as data centers, artificial intelligence (AI), machine learning (ML), and quantum computing, and Samtec’s products and roadmaps are carefully designed to satisfy these high-performance needs. On-Package or ASIC-Adjacent Cable System OSFP 224 Gbps PAM4 … [Read more...]
New High-Performance 90 GHz Test Solution Enables 224 Gbps PAM4 SerDes Characterization
The demand for bandwidth is pushing the limits of test and measurement to speeds and fidelity not previously possible. Complex systems, such as 5G and 6G networks, high-speed SerDes, automotive radar, artificial intelligence, machine learning, and augmented and virtual reality, require much higher frequencies for evaluation. Even though 112 Gbps PAM4 is just now becoming fully available within the market, 224 Gbps PAM4 SerDes characterization is already knocking at the … [Read more...]
Samtec’s First 224 Gbps PAM4 Live Product Demonstration
There’s no end to the demand for bandwidth. Everything from 5G networks, streaming video, social media, augmented and virtual reality, and artificial intelligence and machine learning, are all pushing current-bandwidth limits. The next level is 224 Gbps PAM4. Visitors at DesignCon 23 saw promises and glimpses of 224 Gbps equipment and components. We are excited that we debuted our first 224 Gbps PAM4 live product demonstration. In this video, Ralph Page, Systems Architect at … [Read more...]
Overcoming The Challenges of Achieving 224 Gbps Performance
In this video from DesignCon 2022, Keysight's Mike Resso refers to 224 Gbps as a "blindingly fast speed." Ten years from now, when 224 is old-hat and commonplace, we will look back at that statement and smile at how far we've come since those technologically backward, archaic days of 2022. But as of today, achieving that data rate is bleeding-edge and state-of-the-art. This video, with Mike and Samtec's Jignesh Shah, discusses several topics related to 224 Gbps performance, including ... … [Read more...]
Convergence: A Key to 224 Gbps PAM4 System Design
Convergence in technology is not a new idea; it infers that disparate technologies evolve to a closer association or integration over time. Many believe convergence is required for future 224 Gbps PAM4 system performance. Samtec’s Scott McMorrow and Matt Burns recently authored the article “Convergence: Key to 224 Gbps PAM4 System Design” for Signal Integrity Journal. It’s worthwhile to read the entire article, but if time doesn’t permit, the rest of this blog is a summary of the key … [Read more...]
- 1
- 2
- 3
- …
- 8
- Next Page »