Are you headed to DesignCon 2024? If yes, be sure to stop by the Samtec Booth (#939) to see demonstrations of products that address interconnect needs all the way up to 224 Gbps. New and established Samtec products on display will include those used in front-panel, mid-board, and backplane applications, including our new backplane solutions, optical mid-board options, and test point system.
Look for our green shirts at the Welcome Reception on Tuesday and say hello! Try to make some time to see Samtec engineers engage in their 11 papers, panels, and presentations throughout the conference.
Booth Demos take Center Stage
Samtec is set to reveal a dynamic array of high-speed interconnect products at Booth #939 during DesignCon, ready to usher in the new era of high-speed connectivity. Showing front panel, mid-board, and backplane applications, Samtec’s booth will feature collaborations with Alphawave Semi, Cadence, Keysight, Microchip, Multilane, Rambus, Rohde & Schwarz, and Synopsys, with active 112 Gbps and 224 Gbps demonstrations.
Samtec’s DesignCon booth will spotlight new products for 224 Gbps systems. Starting at the front panel, offerings include Flyover® SFP, QSFP, OSFP, and Samtec’s proprietary NovaRay® IO.
Mid-board solutions will include: Si-Fly High Density (HD), Si-Fly Low Profile, NovaRay, and Accelerate® HD. Moving from mid-board to the backplane, Samtec introduces Si-FlyTM Backplane and NovaRay Backplane alongside existing families ExaMAX® and Xcede® HD.
We are excited to also show you our optical mid-board options, including FireFlyTM and the newly introduced HaloTM. These products will connect with partner platforms through Bulls Eye®, Samtec’s precision RF test point system, with a new Bulls Eye® 90 GHz version. Demonstrations will not only activate the products electrically but also mechanically, showcasing the stability and reliability of the systems and components.
Samtec products will also be part of active 112 Gbps and 224 Gbps demonstrations in partner booths – Keysight, Cadence, and Rohde & Schwarz.
More details on Samtec’s participation at DesignCon 2024 can be found at www.samtec.com/designcon. We look forward to seeing you there!
Also See:
Samtec Experts on Stage at DesignCon 2024 – The Samtec Blog
New 224 G Interconnect Family In A Live Product Demonstration – The Samtec Blog
An Optical Illusion? Maximum Signal Density and Design Flexibility – The Samtec Blog
Leave a Reply