OFC 2020: The Show Must Go On

OFC 2020 Demo Collage

Since we missed OFC 2020 and the opportunity to meet with our customers and blog readers in person, we decided to bring the show to you. We had an incredible booth planned with six live product demonstrations and multiple new product introductions. 

OFC has always been the single best place in the optics industry to meet with customers and partners, address the technical challenges with next generation systems, and demonstrate Samtec’s industry leadership. This time we had planned to demo multiple high-speed copper and optical interconnect solutions at speeds up to 56 and 112Gbps PAM4

Our engineering team put together a series of videos that gives very brief overviews of the key product demonstrations that we had planned for OFC 2020. So, sit back and enjoy the show!


Direct Connect™ To Silicon Package

Samtec Direct Connect™ technology enables 56 Gbps PAM4 and 112 Gbps PAM4 systems that eludes BGA traces. With Direct Connect, Samtec Flyover® cable assemblies plug directly into the package. This is an enabler for many other technologies, including AI, machine learning, 5G, emulation, and high-performance computing.

Si-Fly™ is a new, Direct Connect 112 Gbps PAM4, low-profile, high-density cable system. 


112 Gbps PAM4 QSFP-DD Connector System Enabled By Samtec Flyover

This demo, a collaboration between Samtec and Alphawave, emulates next generation data center equipment architectures, and incorporates Samtec Flyover® to improve signal integrity and architectural flexibility. Samtec Flyover routes critical high-speed signals from the ASIC, above lossy PCB materials, directly to the panel, utilizing ultra-low-skew twinax cable


PCIe® Over Fiber

In this application, instead of inserting a video card directly into the host system PCI Express slot, a FireFly™ optical interconnect allows the motherboard PCI Express bus to be “extended” to a remote location. Products and technologies featured in this demonstration include Samtec FireFly the PCUO series and the PCOA add-on card.


Immersion Cooling of Optical Transceiver, PCB

This is a live demonstration of an immersion cooling system with a submersible optical Samtec FireFly transceiver running at 112 Gpbs (x4-28 Gbps/lane). Next generation super computers, quantum computing, AI engines, and high-performance emulation systems are all evaluating the benefits of liquid cooling.


Connector Systems For AI Hardware Design

Ralph Page walks us through a live demonstration of a prototypical AI (artificial intelligence) hardware design. It’s a configurable, next-generation, possibly GPU-based system that combines a cable mesh backplane, a rigid-style backplane, high-speed edge card connectors, and precision RF interconnects. Products discussed include the AcceleRate® high-speed cable system and HSEC6 edge card connector system.


Salt-Fog Resistant Connector Systems

This proprietary Samtec solution makes both Samtec copper and optical FireFly connector systems salt and fog resistant. It’s particularly beneficial for aviation and military industries.

Here’s a link if you want to learn more about the Samtec products and technologies that were going to presented at OFC 2020.

You May Also Enjoy:

Leave a Reply

Your email address will not be published. Required fields are marked *