New Rugged, High-Speed Twinax Cable Solutions


High-Speed Twinax Cable Solutions To 224 and 112 Gbps PAM4

At DesignCon 2024, Samtec had several live product demonstrations showing a wide variety of Samtec Flyover® cable solutions, all with excellent performance at 224 and 112 Gbps PAM4 data rates. One thing they have in common is Samtec’s Eye Speed®, ultra-low skew twinax cable.

Eye Speed is Samtec’s proprietary, co-extruded twinax cable that optimizes signal integrity, bandwidth, and reach. Because of our unique manufacturing process, Samtec Eye Speed cable is ultra-low skew, meaning the performance doesn’t vary when the cable bends. 

In the video above, Samtec’s Andy Shrout quickly walks us through three live product demonstrations at DesignCon 2024.

112 Gbps PAM4 While Subject To Dynamic Flexing

HDRcade - 112 G - DC24 - Samtec - High Speed Twinax V2

The first, which received a lot of attention, shows the superior performance, as well as the ruggedness, of Eye Speed twinax. And, it’s fun.

An Alphawave Alphacore SerDes delivers 112 Gbps PAM4 signals, which are then run through a long-reach cable system that is subjected to dynamic flexing. The Eye Speed cable runs through the Samtec “HDR-Cade” game, where it bends, twists, stops, starts, and receives all kinds of harsh and rugged treatment. 

That’s because the cable flexing is controlled by whoever is playing the game. Despite this brutal treatment, the cable performance is great. We see a BER of e-8. Most importantly, there are no spikes. And remember, we’re taking these measurements in real-time while we’re bending the cable.

HDRcade-Eye-Speed-Performance-DC2024-Samtec-High-Speed Twinax

BTW, the NovaRay® I/O cable being flexed in the arcade is three meters long. 

High-Speed Twinax Cable Solutions: 224 Gbps PAM4

Samtec Eye Speed twinax cable is also used in all of our 224 Gbps PAM4 DesignCon demos. 

Next in the video, we see a demo that incorporates a Rohde and Schwarz ZVA 110 VNA.  The VNA measures insertion loss all the way to 110 GHz, through a Samtec Si-Fly® HD cable assembly. The loss is flat until 80 GHz, and there’s no suckout. Excellent performance!

Samtec Rohde and Schwarz 110 VNA 224 Gbps SiFly HD DesignCon 2024 Wide

Lastly in the video, we see a live product demonstration where a Synopsys 224 G Ethernet PHY is transmitting 31-bit, PRBS data at 224 Gbps PAM4. The signal travels through the Samtec Si-Fly HD cable assembly, which incorporates 20” of Eye Speed Ultra Low Skew Twinax, then to a second Synopsys 224 G PHY for analysis.

Synopsys Samtec 224 Gbps SiFly HD DesignCon 2024 Wide

The results are impressive, with a PRE-FEC BER of e-6. The total loss is approximately 40 dB at 56 GHz. The loss attributed to the Samtec cable assembly and two characterization boards is 29 dB. And remember, this cable assembly is over half a meter long, at 224 Gbps.

Synopsys 224 Gbps SiFlyHD DesignCon 24

Samtec Eye Speed Twinax cable has better loss characteristics than PCB transmission lines. This is because of the dielectric material used, as well as the electrical properties of the conductor.  

If you have any questions about any of the demonstrations discussed today, contact us at [email protected]

You May Also Enjoy:

Leave a Reply

Your email address will not be published. Required fields are marked *