Embedded World 2019 is the conference for security in electronic systems, distributed intelligence, the Internet of Things / e-mobility, and energy efficiency. In other words, you are going to experience a wide range of embedded systems. It shouldn't come as a surprise, since we are writing about it, that Samtec will be an exhibitor at the conference. This year, Samtec is showcasing the 28 G Product Demonstrator and the full line of products that enable our customers to achieve their goals in … [Read more...]
Mechanical Shock and Vibration and Your System
Using a connector set that hasn't been tested for mechanical shock and vibration is like getting a tattoo on your face while jumping on a trampoline; probably isn't a good choice. Ok, maybe you are thinking, "I'm an engineer, and everyone knows engineers don't get tattoos." Well if you can't relate with that, then maybe you can relate with needing a connector set that can withstand rough handling, transportation, and conditions that aren't static. What Are We Measuring? Mechanical … [Read more...]
Experience “Samtec Live” at our Silicon Valley Design Center
They say that proof is in the pudding, and Samtec invites you to come and see our pudding. Samtec is always looking for ways to provide a higher level of service to our customers, and having all of our demos in one spot is just another example. What Will You See? If you have been following this blog for any amount of time, then chances are likely you have seen some of the amazing demos Samtec has released. Some of our most recent demos have found a home at Samtec SVDC right in Silicon … [Read more...]
Current Carrying Capacity
It was hot, really hot. In fact, things were getting so bad the walls around us were starting to melt, and just like that it was over; we failed current carrying capacity. That is Current Carrying Capacity (CCC) in a nutshell, well it would be if the parts were failing. Samtec performs this in-house during the qualification testing for all product series. What is Current Carrying Capacity? Current Carrying Capacity (CCC) is used to establish the maximum current carrying capacity … [Read more...]
Fan-Out Wafer-Level Packaging
Advances in packaging have afforded companies the ability to place a larger number of contacts in smaller footprints, improve the thermal characteristics, and improve the electrical performance of their systems. One of these advances comes in the form of Fan-Out Wafer-Level Packaging (FOWLP). FOWLP offers an improvement over wafer-level packaging (WLP), and was developed to provide a greater number of external contacts with a silicon die. How does it work? The … [Read more...]
Insulation Resistance and Dielectric Withstanding Voltage Testing
That’s shocking! Insulation Resistance and Dielectric Withstanding Voltage are two of the qualification tests that Samtec performs in-house during part qualification testing. These tests will ensure that when a connector is used in environmental conditions at the rated working voltage (de-rated from the test voltage) the product will not fail, and there will not be current leakage. Insulation Resistance Testing The purpose of the Insulation Resistance (IR) test is to determine the … [Read more...]
Integrated Circuit Packaging and GCT
If you aren’t from the packaging world, then chances are likely you might think “packing” refers to objects being placed in to a box instead of packaging integrated circuits (IC’s) on a substrate. Packaging has advanced since it began, and as with many areas it is all in effort to save space, obtain faster speeds, and to lower costs. Without advances in packaging, we can’t get smaller phones, medical implantables and wearables, or even smaller sensors on an autonomous car. 2D, 2.5D, and 3D … [Read more...]
Samtec, COTS, and Mil/Aero
When it comes to the Military / Aerospace industries, you probably think of products that are rugged and meant to take abuse. The products used in these industries are required to operate and last in extreme environments, and product testing is as important as the product itself. Because of the extensive testing requirements, the cost of a product can be considerably higher and have a longer lead-time when compared to a commercial version of the same product. Why Samtec for … [Read more...]
Wishing for “Normal” Force
What is normal? Anyone with teenagers has probably been asked to be normal. Perhaps that is due to your “normal” protein intake being when you “snap into a Slim Jim,” or how you consider unpackaged circus peanuts a “normal” handout for Halloween. In either case, one might get your house pranked, and neither are applicable to the topic at hand, normal force. What is normal force? Normal force is a perpendicular force to the surface of contact. To help you visualize this, the free body … [Read more...]
Samtec Releases New Video for Glass Core Technology
As with many things, nothing stays the same; especially in the world of technology. Samtec continues to improve and refine its offerings with Glass Core Technology (GCT), and with that there is also a need to update the materials surrounding it. Tell me more Through Glass Vias (TGV), Redistribution Layer (RDL), and Microchannels and vias all play a part in Samtec's ability to provide customers with GCT allowing miniaturized designs and increasing performance. Below are the … [Read more...]
- « Previous Page
- 1
- …
- 3
- 4
- 5
- 6
- 7
- Next Page »