Developing with FPGAs requires patience. Why? They are so flexible and configurable. System designers are only limited by their imagination. Prototyping with FPGAs also poses many challenges. It seems like there are new FMC / FMC+ solutions appearing daily. Sometimes the FPGA carrier card or development board can get crowded. How can that be fixed? VITA 57.4 FMC+ Extender Card Engineers prototyping with industry-standard FPGA evaluation and development kits often leverage the FMC+ … [Read more...]
New Optical FMC+ Module Supports Extended Temperature Ranges
Readers of the Samtec blog are familiar with the benefits of FMC and FMC+. These popular interfaces define a compact electro-mechanical expansion interface for a daughter card to an FPGA baseboard or other device with re-configurable I/O capability. VITA 57.1 has been around for some time. It supports 10 full-duplex transceivers running at 10 Gbps. The new VITA 57.4 standard defines two new connectors. Combined, they offer 32 full-duplex transceivers running at 28 Gbps. New … [Read more...]
Samtec Releases New VITA Standards Webpages
As a connector company, Samtec is involved with a wide variety of different Industry Standards and Protocols that are constantly growing. From USB to PCI Express, Standards allow for our compliant interconnect solutions to be deployed in a diverse number of configurations and settings. One of the largest Standards families Samtec participates with is VSO, VITA Standards Organization, better known as just VITA. VITA members have worked together to define and develop key computer … [Read more...]