PLDA and Samtec Demonstrate PCIe 4.0 over FireFly™ Micro Flyover System™

PLDA and Samtec recently announced a demo of their combined PCIe 4.0 solution that delivers full PCIe 4.0 bandwidth (16 GT/s) over copper or optical fiber at minimal cost.
The joint demonstration combines PLDA’s PCIe 4.0 IP solutions with Samtec’s FireFly™ Micro Flyover System™.
It delivers PCIe 4.0 speed without the use of retimers or updated motherboard using MEGTRON 6 other exotic laminates.
This demo suggests a solution to overcoming the inherent limitations of maintaining PCIe 4.0 performance over long distances without changing the motherboard technology or using costly retimers.
New PCIe 4.0 Applications
As cloud computing and deep learning accelerators drive faster advances in the PCIe roadmap, existing hardware designs cannot support the higher speed signals over the same distances. The PCIe 1.0 specification allowed signals to travel as much as 20 inches over traces in mainstream FR4 boards, even while passing through two connectors.
In contrast, today’s quicker 16 GT/s PCIe 4.0 signals will peter out in under six inches and without going over any connectors. In today’s designs, PCIe 4.0 signals can only travel three to five inches, requiring costly redesigns, moving to MEGTRON 6 and adding a retimer for increased distance.
Demo Overview and Benefits
The PLDA and Samtec solution demonstrates an alternate approach using optical fiber (330 feet) or Twinax Flyover™ Systems (10 inches) to deliver PCIe 4.0 x4 with no significant loss of bandwidth.
Key benefits include:
- PLDA’s demo shows a system running at 16 GT/s and displaying relevant throughput and latency measurements. The demo result shows the bandwidth is not impacted by distance when using copper or optical fibers.
- By using optical fibers, PLDA and Samtec demonstrate that PCIe 4.0 can be used for remote applications (e.g. EMI sensitive environments)
- By using passive Twinax Flyover™ Systems, PLDA and Samtec show a differentiated and affordable way to design a PCIe 4.0 platform. According to Rick Merritt, adding retimers could cost between $15 to $25 for 16 lanes of PCIe 4.0 at 16GT/s, plus an additional $300 for updating the motherboard PCB material.
“PCIe Designers are delaying their upgrade to the next generation of PCIe because they anticipate high board manufacturing costs, said Hugues Deneux, COO of PLDA. “With this demo, we want to show a new approach that provides great bandwidth and good latency over any distance for PCIe 4.0 communications.”
“Samtec and PLDA’s multi-year PCIe 4.0 collaboration lowers barriers of entry and quickens time to market,” said Arlon Martin, Senior Marketing Director of Samtec Optical Group. “The Samtec PCIe® Optical Flyover Cable Assembly enables designers to more efficiently take advantage of the incredibly low latency and high throughput without board constraints“.
The PLDA/Samtec PCIe 4.0 Demo
This new demo offers a new approach to overcoming inherent distance limitations in traditional PCIe architectures. The video below outlines the key details.
Additonal PCIe 4.0 resources are also available below:
- The joint Samtec/PLDA press release
- Explore multiple silicon proven PLDA’s PCIe 4.0 controller solutions
- Find PCIe 4.0 platform tailored for prototyping, developing and debugging
- Find more information on Samtec’s FireFly™ Micro Flyover System™ at https://www.samtec.com/firefly
- Contact PLDA to schedule a time to test your own hardware using PLDA’s demo at [email protected]