Six Tips To Help You Select The Right Connector

select the right connector - variety of board stacking connectors from Samtec

I’ve worked with many engineers trying to select the right connector set for their board-to-board application. I felt bad for them because they had many options to choose from, and it can be a confusing, frustrating endeavor. It’s made it all the more complicated because no two applications are identical.

This blog aims to give you a few design tips from a connector company veteran (that would be me). These practical, commonsensical suggestions (hopefully) will help you select the right connector set for your application (hopefully). And this isn’t an exhaustive list – these are the first six that came to mind – but we’ve got to start somewhere.

popular connector Rugged, Industrial, Tiger Eye Samtec

Consider The Environment:  In other words, what demands are placed on the connector set?  What is the connector’s lifestyle? Easy or difficult? An example of an easy life is one where the connector system is cycled (i.e., mated and unmated) maybe 10 times or less, and it spends the rest of its life in a climate-controlled room. A difficult life is one that will require multiple cycles, maybe 100, 200, or more, and is subject to shock and vibration, constant movement, high humidity, temperature swings, and/or corrosive chemicals and vapors. Selecting the right contact system is critical to the success of the connector set, especially if your connector is going to live a difficult life.

Connector suppliers like Samtec offer a variety of contact systems, from basic designs for those connectors blessed with the easy life to rugged contact systems for those connectors that have it rough. Since this is a Samtec blog, here’s a link showing you some of those contact systems.  

Consider Normal Force:  One factor that will help you select the right contact is its normal force. Normal force has been called the single best predictor of connector performance. If you are considering two connector systems, and it appears both will work, choose the one with a higher normal force. This is important in harsh environments, and it’s keenly important if the environment experiences extreme temperatures or high shock and vibration. (Here’s another blog on normal force, if you’re interested.)

Consider Insertion Depth:  If you have narrowed your choice to two connector systems, and if you’re happy with the contact design and normal force of each, then another factor to consider is the socket’s insertion depth. The greater the insertion depth, the more stable the board stacking system.

Consider Pin Configuration:  If your design requires 20 pins, use a 2 X 10 connector, not 1 X 20. The longer the connector, the more problems you may experience with coplanarity, alignment, and soldering.

Consider The Centerline (or “Pitch”):  This is mostly a matter of mechanical stability. A fine-pitch connector, meaning one with a centerline of 1.27 mm or smaller, will probably not be sufficient if it’s expected to be the sole means of mechanical stability between large or heavy PCB assemblies. Speaking for Samtec, we have a variety of rugged, microminiature connector systems that are sturdy and well-designed, but you’re still asking for a small component to support a lot of weight and torque.

Of course, there’s more to consider than the six points above when selecting a connector solution. But hopefully, this list serves as a start. If you want to pick our brains about connectors, we’d love to hear from you.

You May Also Enjoy:

Leave a Reply

Your email address will not be published. Required fields are marked *