Here are the April 2022 Website Updates to Samtec.com

We spent most of April finishing up a couple of large applications that were built on legacy code. Those are now updated and live on the website. We also rolled out a couple of content page upgrades, and some back-end speed optimizations to various areas of the website.

New Material Declaration Application

material declaration

We launched a new upgraded version of our Material Declaration application, which allows users to download a digital part composition analysis for any eligible part number. We upgraded the front-end design of the tool, performance, and the design of the PDF it generates.

This replaces a legacy tool with new architecture and code that we had been running since 2012. It can generate up to 50 material documents for download in under a minute.

Take a look at the upgrade here – https://www.samtec.com/tools/material-declaration

New RoHS Application

rohs application

Similar to the above tool, we also launched a new version of our ROHS application, which allows users to obtain a RoHS certificate of compliance for all eligible part numbers. This can be downloaded for China RoHS and European RoHS certificates.

This tool also replaces a legacy tool with new architecture and code that we had been running since 2012. It can generate up to 50 RoHS documents for download in under a minute.

Take a look at the upgrade here – https://www.samtec.com/tools/rohs

New VITA 66.5 Standards Page

vita 66

As an extension of VITA 65 OpenVPX, VITA 66 enables a compatible VPX interface containing blind-mate optical connectors with fixed contacts on the Plug-In Module and floating displacement on the backplane.

VITA 66 allows for improved and diversified I/O density via fiber transceivers and cables. While transceivers can be dense and perform at a high speed, they often consume valuable board real-estate, require additional hardware, and are difficult to integrate due to an ultra-fine pitch.

Samtec compliments the VITA 66 standard by offering our cabled FireFly™ Micro Flyover System™. FireFly™ supports SWaP-C and offers more density and performance (28+ Gb/s) than optical transceivers while consuming less board space.

We recently launched a content page to showcase how we support the VITA 66 Optical VPX Standard with our products and support teams.

Take a look at the new VITA 66 Page herehttps://www.samtec.com/standards/vita/opticalvpx

Mobile Optimizations for Application Pages

applications

The Applications section of our website is fairly new. It showcases how Samtec products are designed-in and applied across a wide variety of industries and technologies, including 5G, automotive, industrial, instrumentation, broadcast video, and more.

We recently optimized all of the pages in this section for mobile use, making them much easier to read and consume on mobile devices.

You can access each page by heading to the main Applications page here, and clicking the panels within – https://www.samtec.com/solutions/applications

Speed Optimizations for Static Pages

about page

We’ve been working on a static website conversion as a lower priority as we are able to bit things off for quite a while now. Samtec.com is huge, and it contains hundreds of static pages that don’t require any code to run. We’ve been slowly moving these out of our main codebase and building CDN-driven versions of them that run extremely fast and require a very small amount of server resources to run effectively.

In April, we converted 20 additional pages throughout the website to run using this technology. Most of these live in our Support and Tools sections of the website.

You can see an example of a page running on this technology here. Notice the incredibly fast page load time you experience when accessing the link – https://www.samtec.com/about

Coming Soon to Samtec.com

That does it for the major web updates this month.

Here is what we’re currently working on, and a few other updates that are coming soon!

  • Continued upgrades to our e-commerce experience throughout the website
  • Updated capabilities to manage profiles online
  • Upgraded checkout features
  • An updated way to find Optical products
  • An updated way to manage orders online
  • A design upgrade to our Mated Set view
  • And more!

Keep an eye out for these updates and more coming soon.

Drop your email address in the form below if you want to stay in the loop with these updates, and as well as the rest of our blog content.

If you have any feedback or suggestions for our web team, feel free to send an email at [email protected].

You May Also Enjoy:

Leave a Reply

Your email address will not be published. Required fields are marked *