As end-applications venture into the sub-Terahertz spectrum, Samtec has recognized the need for a new generation of products, one that incorporates an innovative approach by integrating a cable design that can support frequencies up to 90 GHz (E-band) with loss performance improved over today's coaxial cables. Enter our next-generation micro waveguide technology, offering the near-loss performance of a rigid waveguide while still providing the flexibility and size typically associated with a … [Read more...]
The Diverse Connector Market
The connector marketplace is one of the most diverse and interesting in the entire electronics industry. The roles that connectors are required to play range from the smallest data connections to the largest power supplies. They are frequently employed in some of the toughest conditions on Earth and despite this are expected to provide remarkable levels of reliability. As a result, the industry has responded with a quite bewildering array of choices. Many connectors are designed as … [Read more...]
A New Angle On Power/Signal High-Density Arrays
Angles surround us every day – physical angles like the corner over there, and angles of perspective. Samtec’s new AcceleRate® mP high-density power/signal interconnect system was born out of a different perspective on power integrity and a 90 degree rotation. Best in class density for a power/signal interconnect system, AcceleRate® mP achieves up to 240 I/Os in .438 sq. inches. It also packs a punch with up to 22 Amps per power blade and 56 Gbps signal performance. Rotated Power … [Read more...]
Wideband 24-30 GHz Phased Array Antenna Module Demonstrates Excellent 5G Comms Link
Wideband 24-30 GHz 5G mmWave capabilities are showcased in this demo by establishing an over-the-air (OTA) communication link between two Phased Array Antenna Modules, or PAAMs. Samtec's Jim Alexander walks us through one of several live product demonstrations from IMS 2023. This one is presented with our friends at Otava, Rohde and Schwarz, Taoglas, and Avnet. The modulated 5G FR2 signal is generated using a Rohde & Schwarz SMW200A vector signal generator which is sent to the … [Read more...]
Samtec’s New and Improved YouTube Channel
Hey Google! - "Clink" How do I download a Samtec 3D model? Most times when you are searching a topic, question, or how to do "blank", a YouTube video pops up with a solution. As the second largest search engine and video streaming platform, YouTube has revolutionized the way we consume, create, and share content. Every second of every day videos are being uploaded and posted to YouTube by individuals, media outlets, and major corporations. Samtec recently revamped its YouTube Channel with … [Read more...]
Microwave, mmWave Connector Systems Achieve Excellent Performance
At IMS 2023, Samtec had a booth full of cutting-edge product demonstrations and technologies. One of those featured a variety of microwave, mmWave connector systems which achieved excellent performance. Michael Griesi, RF Design and Simulation Engineering Manager at Samtec, walks us through the demonstrations and the results. A Keysight eight-port 53 GHz USB VNA transmits signals to the four mmWave RF systems. The Keysight device is a M9808A PXIe Vector Network Analyzer (100 kHz to 53 … [Read more...]
Validating the Performance of Miniature Array Connectors
Small, complex, and portable applications (in industries such as military/aerospace and medical) require miniaturized, reliable interconnects. As traditional surface-mount and through-hole interconnects reach their limits in terms of density and the number of signals that can effectively be used, many product designers are implementing high I/O array styles of interconnects. In a new white paper from Samtec, “Improved Solder Joint Integrity for High-Density Interconnect Applications,” the … [Read more...]
New High-Performance 90 GHz Test Solution Enables 224 Gbps PAM4 SerDes Characterization
The demand for bandwidth is pushing the limits of test and measurement to speeds and fidelity not previously possible. Complex systems, such as 5G and 6G networks, high-speed SerDes, automotive radar, artificial intelligence, machine learning, and augmented and virtual reality, require much higher frequencies for evaluation. Even though 112 Gbps PAM4 is just now becoming fully available within the market, 224 Gbps PAM4 SerDes characterization is already knocking at the … [Read more...]
Tradeshows Around the World 2023
We tend to have large write-ups on shows around North America and Europe. As a global company, we have just as many if not more shows all around the world! Many Asian shows are shared through regional channels so not all of our readers may not be aware of other opportunities to share the Samtec experience. Shows around North America slow down over the summer months to kick off strong starting in August. Our team on the other side of the world seems to be very busy between June and July. … [Read more...]
Samtec Sponsors Signal Integrity Projects with Universities
In our increasingly interconnected world, where data transmission and communication play a crucial role, the field of signal integrity as a profession is highly in demand. As electronic devices become smaller, faster, and more complex, ensuring the reliable and efficient transmission of electrical signals has become paramount. Recognizing the importance of this field and for continued education and innovation, Samtec proudly saw a need to sponsor 3 intriguing and unique capstone projects focused … [Read more...]
- « Previous Page
- 1
- …
- 7
- 8
- 9
- 10
- 11
- …
- 62
- Next Page »