No matter where we look the amount of devices connected to the Internet continues to grow. It seems but only a few years ago that a PC with a dial-up 56 kbps modem was bleeding edge. Households with internet connectivity measured in the millions.
According to one source, only 1% of the world’s population had Internet connectivity in 1995. Obviously, times haves changed with smart phones, wearable fitness devices, media players and other commonplace Internet-connected consumer devices. Today, almost half of the world’s population has access to the Internet.
While the growth of wireless networks, inexpensive smart phones and other consumer devices help drive consumer Internet connections, other not-so-intuitive applications are driving the total amount of devices connected to the Internet.
Several research firms predict that enteprise IoT devices, government IoT devices and industrial IoT (IIoT) devices will accelerate the number of global Internet connections faster than consumer IoT devices. Some applications driving this include wireless sensors, industrial communications and connections to the cloud on the factory floor.
In response to these trends, Avnet has released the Avnet MicroZed™ Industrial IoT Starter Kit. This is an out-of-the-box solution giving OEMs a quick path from prototype to production for their IIoT connection needs.

The kit comes with the following:
- MicroZed 7010 SoM
- MicroZed Arduino™ Carrier Card
- Pluggable sensors
- Ethernet, USB and power cables
- Free trial of cloud computing software
The IIoT Starter Kit features various Samtec interconnect solutions including BCS series and SSQ series. For more information on the Avnet Industrial IoT Starter Kit, please see the following links: