Our new DCC Series -- direct connect cable system – is a cost-effective high speed cable solution that supports and surpasses PCIe® Gen3 speeds at 2 meters cable length. The DCC is rugged. High retention press fit pins attach directly to the … [Read more]
Solder Balls On High Density Arrays Self-Align During Reflow
Check out this video of how Samtec’s ZA8 Series, a high density grid array interposer, self-aligns during reflow. We are frequently asked about the placement and processing of high density arrays. As shown above, the self-centering characteristics of … [Read more]
Come to See Samtec At New Tech, Israel
Please visit Samtec at the New Tech Exhibition - 2015, on 19 and 20 of May. We are at booth #40. You can see several of our major new products, including: ExaMAX® backplane systemsZ-Ray™ high density, low profile interposersAdditions to the … [Read more]
High Density Arrays Offer Maximum Design Flexibility
Check out our new SEARAY™ video for a quick overview of why it’s one of the fastest-growing, most robust interconnect systems in the industry. Here’s why: high density (up to 500 I/Os)high speed (28+ Gbps)routing and grounding flexibility (open … [Read more]
SEARAY™ Solder Joints Are Class 3, IPC-A-610
Samtec SEARAY™ SEAM, SEAF Series solder joints are now classified as Class 3 in the IPC-A-610 Rev F Standard. Class 3 is for high performance/harsh environment electronic products. This includes products where continual high performance or … [Read more]
Samtec Joins IRT Nanoelec Silicon Photonics Program
Samtec is pleased to announce its entrance in the Silicon Photonics Program of the IRT Nanoelec headed by CEA-Leti. Samtec is joining CNRS, STMicroelectronics, Mentor Graphics and CEA-Leti to develop and industrialize optical communications solutions … [Read more]
Z-Ray® Ultra Low Profile, High Density Interposers Provide Design Flexibility
Samtec’s Z-Ray® one piece arrays are ultra-low profile, high density and highly customizable compression contact arrays used as interposers or as board level interconnects. Compared to standard interposers, they feature greater density, X-Y-Z axes … [Read more]
Samtec 12 Channel, 28G FireFly Demo – An Interview With Kevin Burt
Check out this video from OFC, with Samtec's Kevin Burt discussing the demo of our FireFly™ 12 channel optical Micro Flyover™ System operating at 28 Gbps/channel (336 Gbps aggregate). Kevin also discusses the benefits of mid-board optics. … [Read more]
28 Gbps FireFly Demo With Anritsu MP1800A At OFC
Anritsu Company (OFC booth #1309) and Samtec (OFC booth #1849) are conducting optical transmission technology demonstrations in the Samtec booth during OFC 2015, in Los Angeles, March 24-26. The demonstrations use high quality signals generated from … [Read more]
Be Sure to Visit Samtec at OFC
We hope you can visit us at OFC, March 24-26, at the Los Angeles Convention Center. Our booth (#1849) will have two high-speed product demonstrations and onsite experts to bring you up-to-speed about several new Samtec products. Our physical … [Read more]