Samtec recently worked with our friends at Powell Electronics on a little marketing piece. The goal is to showcase our partnership related to Defense and Aerospace specific products Samtec supplies. Working with another family-owned, US-based company allows us to understand some of the nuances associated with the defense and aerospace industries.
Any way that we can continue to grow our presence in the marketplace helps not only Samtec but the industry as a whole. A US-based manufacturing, Sudden Service, COTS Products Reserved for the customer and ready to ship the next day, through multiple channels makes for a fantastic combination for the Defense Industry where a warfighter’s life is on the line when technology is not there and ready for them.
QuickChat with Powell and Military + Aerospace Electronics
We were excited to sit down with Jamie Whitney, Senior Editor at Military & Aerospace Electronics and have a conversation about how Samtec supports the industry with Powell’s help.
QuickChat: COTS products with SWaP in mind for Defense and Space applications
Lot Screen Testing to MIL-DTL-55302
A recent addition to how Samtec supports Defense and Aerospace industries is by implementing a sample-sized Lot Screen Test. We touched on this in the conversation with Jamie, but are excited to add this to our lineup. Years ago Samtec introduced SET (Severe Environment Testing) to some of our design qualifications. (see the link below for additional tests added at that time)
The introduction of SET was a great baseline when introducing a product to the market. Lot screen sample testing is the next level. This is where some of these more rigorous inspections are added with every lot of assemblies built. Working with Powell, and key customers, we were able to identify critical aspects of the MIL-DTL-55302 and implement this within the production line.
How can I Learn More or Request MIL-DTL-55302?
If you skipped over the video above scroll back up and listen in to the quick 10-minute conversation. If you are ready to ask for support on general Military and Aerospace products follow either of these links:
- Reach out to samtecinfo@powell.com to speak to an expert.
- Navigate to Powell’s site here Samtec Military Aerospace Market Offerings | Powell Electronics
Curious about setting up custom routings to include a sample MIL-DTL-55302 report with an order reach out to the Samtec team direct at Military@samtec.com. We are happy to help you understand how we can not only provide sample Lot Screen Testing but also help you with;
- Modified COTS Built to Samtec’s Print
- Manufacturing Location Control Available
- Product Specification Control Available
- Non-Standard Options Available
- AS9102 FAI Available
- ITAR Control Available

Additional Tests Included with SET:
- VITA 47.1 Module Insertions
- VITA 47.3 Humidity
- VITA 47.1 Operating Shock Class OS2
- VITA 47.1 Vibration Class VS3
- Exceeds VITA 47.1 Temperature Cycling Class C4
- Exceeds VITA 47.1 Non-Operating Temperature Class C4
- VITA 47.1 Electrostatic Discharge Resistance
- Exceeds VITA 47.1 Altitude for DWV
Leave a Reply