Testing the Effects of Humidity on Connectors

Many electronics experience a wide range of climates while in operation and storage. Because of this fact, connector humidity testing is used to determine the ability of a product to withstand elevated humidity and cycling temperatures.

Humidity testing is conducted in combination with other qualification tests; mating / un-mating, Low Level Circuit Resistance (LLCR), and Insulation Resistance / Dielectric Working Voltage (IR / DWV).

What is Connector Humidity Testing?

Since condensation on a part can cause failure, it is important to understand the capabilities of the connector set you are looking at using. Failure from humidity can come in the form of corrosion on the plating, and lead to degraded electrical performance.

Humidity testing takes that into account by exposing the mated connector set to a varying range of temperatures, 25°C – 65°C, with a humidity range of 90% RH – 98% RH over 10 days.

How is it Tested?

connector humidity testing
Humidity Test Chamber

In order to determine how the connector set reacts to humidity testing, the parts will go through, mating / un-mating, IR / DWV, and LLCR pre and post humidity exposure.

The connector set is soldered onto the appropriate test boards, and the initial base line test is performed.

The parts are then subjected to the humidity test in the chamber, and then retested to determine if they survived the humidity test.

If connector set does not pass the electrical requirements of LLCR or IR / DWV then the connector set is considered to have not passed humidity testing.

Samtec uses the standard EIA-364-31 “Humidity Test Procedure for Electrical Connectors and Sockets” as the test standard for humidity testing.

Samtec publishes all of its reports on www.samtec.com and can be found according to the series pages. To see the qualification test report that includes humidity test results for the SEAM/SEAF series please click here, or type in the series name of the part you are interested in on samtec.com.

You May Also Enjoy:

One Comment

  1. “Degraded electrical performance” might be the least of your issues when dealing with connectors and water (whether the water comes from condensation or anything else). When there is a voltage potential between connector contacts and a water bridge forms between them, electrolytic corrosion will occur. As current flows through the water, material will be removed from the contact with the higher potential (positive voltage) and deposited along the path to (or onto) the other contact. This may cause a short circuit and will definitely corrode the more positive contact.

    Related trivia: (1) This is the same mechanism that is used intentionally to electroplate things (depositing material on the part with the negative voltage). (2) Salt water is “more corrosive” in the sense that it has less resistance and therefore conducts more current, speeding up the corrosion. (3) Dielectric grease can help by making it less likely that a water bridge will form. (4) If during testing you apply a voltage between connector contacts and any current flows, you know that corrosion will eventually occur under those conditions.

    Galvanic corrosion is closely related. Take two types of metal connected by a (at least slightly acidic) water bridge. That forms a battery. Now let the two pieces of metal touch each other to complete the electrical circuit. Current will flow, and you have the original corrosion issue without needing an external voltage source (although you do need different types of metal). Consider what might happen if you scratch a hole in the plating of a contact so the base material is exposed. Or you use mating connectors with different types of contact plating (e.g. one silver, one tin).

    I might have over-simplified some things, but the point is that your connectors might need to be more waterproof than you think.

Leave a Reply

Your email address will not be published. Required fields are marked *