As data rate requirements approach and surpass 112 Gbps PAM4, developers are challenged with balancing increasing throughput, scalability and density demands with concerns such as power consumption, signal integrity, cost and time-to-market. Samtec helps address these challenges with industry-leading expertise in high-performance interconnect design, and innovative strategies and technologies for the demands of next generation data transmission.
The following are links to live product demonstrations, products, and technologies, that are on display in the Samtec booth at the OCP Virtual Summit.
LIVE PRODUCT DEMONSTRATIONS
Direct Connect™ To Silicon Package
Samtec Direct Connect™ technology enables 56 Gbps PAM4 and 112 Gbps PAM4 systems that eludes BGA traces. With Direct Connect, Samtec Flyover® cable assemblies plug directly into the package. This is an enabler for many other technologies, including AI, machine learning, 5G, emulation, and high-performance computing.
Si-Fly™ is a new, Direct Connect 112 Gbps PAM4, low-profile, high-density cable system.
112 Gbps PAM4 QSFP-DD Connector System Enabled By Samtec Flyover®
This demo, a collaboration between Samtec and Alphawave, emulates next generation data center equipment architectures, and incorporates Samtec Flyover® to improve signal integrity and architectural flexibility. Samtec Flyover routes critical high-speed signals from the ASIC, above lossy PCB materials, directly to the panel, utilizing ultra-low-skew twinax cable.
A Connector Solution To Achieve 112 Gbps Data Rates
As data rate requirements approach and surpass 112 Gbps PAM4, developers are challenged with balancing increasing throughput, scalability and density demands with concerns such as power consumption, signal integrity, cost and time-to-market. This video explains how Samtec Flyover addresses these challenges.
Chassis-to-Chassis, Mid-Board Connectivity Via 5 Meter Cable Backplane
A popular demonstration at Super Computing 2019 (SC19) was a collaboration between Samtec and eSilicon that emulates next generation data center architectures for typical 19 inch rack-mount applications.
HIGH-SPEED PRODUCT SYSTEMS
Flyover QSFP-DD Flyover QSFP28 Cable Systems
Si-Fly™ 112 Gbps PAM4, Low Profile, High Density Cable System
Samtec Flyover Systems For Next Gen Speeds
NovaRay® 112 Gbps PAM4 Extreme Density Arrays
ExaMAX® HIgh-Speed Backplane System
FireFly™ Copper and Optical Micro Connector System
AcceleRate® Slim Body Direct Attach Cable Assemblies
IF YOU’RE IN THE AREA …

Samtec Silicon Valley is located near the Santa Clara Convention Center, the traditional home of the OCP Summit. When our business lives return to normal, or return to our new normal, you are welcome to swing by our office for a tour of our variety of 112 Gbps PAM4 live product demonstrations. These demos incorporate a variety of products and design configurations. You can reach us at HSC@samtec.com.