In the last blog on Severe Environment Testing (SET), we covered "why" and "what" Samtec was testing on its connectors. In this one, we are going to look a little bit further into the "how." Electrostatic Discharge and Dielectric Withstanding Voltage at an altitude of 70,000 ft will be discussed as part of two new tests being performed under Severe Environment Testing. What is new? Electrostatic Discharge Typically, with connectors Electrostatic Discharge (ESD) is not tested. … [Read more...]
Severe Environment Testing for Connectors
With the advent of the Commercial Off-The-Shelf (COTS) part being used in Mil / Aero, Space, Industrial, Transportation, and Automotive applications; manufacturers find themselves still looking for information on how those products will perform in severe environments. Here at Samtec, we have recognized the need for more information about our COTS products, and that is why we have introduced Severe Environment Testing (SET). What is Severe Environment Testing? Severe Environment … [Read more...]
Samtec Expands VITA 57.4 with FMC+ Extender Card
Developing with FPGAs requires patience. Why? They are so flexible and configurable. System designers are only limited by their imagination. Prototyping with FPGAs also poses many challenges. It seems like there are new FMC / FMC+ solutions appearing daily. Sometimes the FPGA carrier card or development board can get crowded. How can that be fixed? VITA 57.4 FMC+ Extender Card Engineers prototyping with industry-standard FPGA evaluation and development kits often leverage the FMC+ … [Read more...]
Testing the Effects of Humidity on Connectors
Many electronics experience a wide range of climates while in operation and storage. Because of this fact, connector humidity testing is used to determine the ability of a product to withstand elevated humidity and cycling temperatures. Humidity testing is conducted in combination with other qualification tests; mating / un-mating, Low Level Circuit Resistance (LLCR), and Insulation Resistance / Dielectric Working Voltage (IR / DWV). What is Connector Humidity Testing? Since … [Read more...]
Are You In a Harsh Environment for an Electronic Device?
Modern electronic devices are getting smaller with every new generation, and as a result, they are becoming more portable. At the same time, the performance of these devices is growing as the demands of consumers become greater. We expect to be able to connect to the internet wherever we go, and so we carry our cell phones, smartwatches and portable devices everywhere. Equipment manufacturers are keen to tell us that our new device will work in harsh conditions, but what does that … [Read more...]
Extended Life Testing for Connectors
They say, "a diamond is forever," but did they really test that or is it just a marketing statement? No need to search for that answer because we all know they didn't. However, in our industry it is important to know what to expect out of a connector, and that is why Extended Life Testing exists. Extended Life Testing tells a system designer what they need to know about a connector set that will be heavily used. This test throws everything but the kitchen sink at it, and who knows, maybe … [Read more...]
A Day In The (Extended) Life: Extended Life Products
Many EOEMs, especially those in the industrial and telecommunications industries, require their connectors be subject to additional, more stringent performance testing beyond the connector’s standard qualification tests. Their applications may require high cycle connectors, exposure to harsh environments, or be expected to perform over a much longer life expectancy than the average connector. High Cycle Connectors Let’s say it another way … few connector sets are subject to 2,500 – … [Read more...]
Gas Tight Testing for Connectors
Gas tight testing falls into the qualification testing that Samtec performs on all products prior to their release. It is not a one and done test, and it uses some of the tests that we have previously discussed as part of the test sequence. As you would probably guess, this test uses a gas to expose any inefficiencies in the system being tested, and the methods behind that will be explored in this blog. What is Gas Tight Testing? Gas tight testing isn't an island all to itself, … [Read more...]
Micro, Rugged Industrial Connectors: Do They Exist?
The Loch Ness Monster? There's that old, grainy picture. Big Foot? I've seen the video. UFO's? Who knows? But micro, rugged industrial connectors? Come on, that's really hard to believe ... But, industrial electronics is Samtec’s largest selling industry sector, and that's because Samtec has a full line of micro, rugged industrial connectors. Applications include factory automation, embedded computing, robotics, monitoring, vision systems, measurement, motion and process controls, and … [Read more...]
An Eye Catching High Performance Test Point System
Samtec Bulls Eye® test point systems are ideal for high-performance test applications because of their compression interfaces, small footprint, and high cycle count capabilities. Bulls Eye is now available in 50 GHz and 20 GHz designs, with a system up to 70 GHz in development. Bulls Eye is a popular product because: The grid design and smaller footprint enables smaller evaluation boards and shorter trace lengths. The high-density array design significantly saves PCB space compared to … [Read more...]