COPLANARITY AND STENCIL THICKNESS STUDY Samtec and Phoenix Contact recently completed dual studies that show when PCB processing requirements dictate using a 0.10 mm (.004”) stencil, the coplanarity requirements for most connectors can be relaxed to a maximum of 0.15 mm (.006”). In other words, Samtec and Phoenix Contact both successfully soldered PCB connectors with 0.15 mm coplanarity using a 0.10 mm thickness stencil with optimized apertures. CHALLENGE FOR DESIGNERS Designers … [Read more...]
Samtec Mezzanine Strips Featured in New MCU Eval Board
Pundits in the semiconductor industry consistently debate the status of Moore's Law. Does it still apply? For how long? How will x86 architectures be affected? These are ongoing questions and concerns for Wall Street and Silicon Valley. The answers will have economic, technological and societal impacts. However, not all end-market electronic devices require a server CPU coupled with a GPU or FPGA accelerator. Sometimes, just a standard, general purpose microprocessor will do. ST … [Read more...]
Samtec, Connectors, and IoT
Chances are likely that you have heard of the Internet of Things (IoT) by now. On that same chance, you have probably heard it so many times that it is starting to become like any other buzzword. I say that in jest however, but just wait until IoT hits the late night infomercial buzzword list alongside the tactical cane with the LED handle that is connected via 5G with your HD vision sunglasses. Where is Samtec in IoT? All jokes aside, IoT and Industrial Internet of Things (IIoT) … [Read more...]
Using Nanosecond Event Detection to Identify Effects of Mechanical Shock and Random Vibration
In the video above, it might not appear that much is taking place, but just like with transformers there is "more than meets the eye." Alright, that was corny, and I am mildly ashamed, but Nanosecond Event Detection for shock and vibration is nothing to be ashamed of testing. Maybe your system operates within highly dynamic environment, and it is important that you don’t experience any interruption in your signal. This is where Nanosecond Event Detection comes into play. What Does … [Read more...]
Samtec Releases New 5G Applications Solutions Guide
"So, what really is 5G?" That may be a question some folks are asking themselves. Why? No one has really heard of any 5G applications yet. Right? Insert rolling eye emoji here. In case someone lives under a rock, "5G" refers to the next-gen cellular standard that will take over the world in 2019 and coming years. 5G offers high speeds and lower latency for improved services such as: IoT/IIoT ConnectivityHigh-speed internet connectivityStreaming Ultra HD 3D videoLonger battery life in … [Read more...]
New Zynq UltraScale+ Platform Offers 32 Gbps via FMC+ and FireFly™ Interfaces
One of the most popular interfaces in the FPGA world is FMC. This has recently been expanded to FMC+. The new VITA 57.4 standard defines two new connectors. Combined, they offer 32 full-duplex channels running at 28 Gbps. However, the current generation of FPGAs and MPSoCs have transceivers supporting data rates in excess of 32 Gbps. Why? Emerging protocols – including PCIe Gen 5 and JESD204C – will run at 32 Gbps. Engineers developing solutions using 32Gbps+ protocols need … [Read more...]
56 Gbps, 5 Meter Backplane Cable Assembly Demo
A joint demonstration between Samtec and eSilicon -- an eSilicon 7 nm 56 Gbps DSP SerDes over a Samtec 5 meter ExaMAX® backplane cable assembly -- caught a lot of attention at SC18. The demo showed a true long-reach capability with a high-performance, flexible, easy-to-configure SerDes that targets common data center standards and data rates. In this video Samtec’s Ralph Page and eSilicon’s Roberto Massolini walk us through the demo, explaining the logistics and the results … [Read more...]
Evaluation and Development Kits Viewable Across Samtec.com
Over the past few years, Samtec has expanded its portfolio of Evaluation and Development Kits. Engineers and designers demand the best tools for system prototyping. From concept and prototype to development and production, Samtec-designed Evaluation and Development Kits featuring high-speed interconnect solutions to help simplify design. Helpfully, they reduce time to market for hobbyists, tinkerers, start-ups and OEMs alike. Easy Access via Landing Page Engineers want instant access … [Read more...]
Increasing Broadband Interconnect Characterization
Samtec's Gustavo Blando recently presented "Increasing Broadband Interconnect Characterization" at EDI CON 2018 in Santa Clara, California. A video of the workshop is above, and below is Gus's summary of his presentation. VNA measurements are the backbone of any SI analysis, both for correlation and basic interconnect understanding. As bit rate increases and specs tighten, accurate measurement at higher frequencies is of paramount importance. For convenience, a coaxial style connector is … [Read more...]
High Speed Interconnect Demos At Electronica 2018
Samtec's full line of high speed interconnect products was on display and in demonstrations at Electronica 2018. Focus products included high speed mezzaninehigh speed cable assemblieshigh speed backplane connectorsactive optical cable assemblies Two of the demos that caught a lot of attention were the 28 G Product Demonstrator and the REFLEX CES Sargon Stratix 10 FPGA FMC+ IDK. 28 G Product Demonstrator In this video, Samtec's Neil Potter walks us through the 28 G … [Read more...]
- « Previous Page
- 1
- …
- 8
- 9
- 10
- 11
- 12
- …
- 22
- Next Page »