As bandwidth requirements become more difficult to route over any distance through a lossy PCB, system architects now have an alternative signal path strategy through Samtec Flyover™. Samtec Flyover™ designs break the constraints of traditional signaling substrate and hardware offerings, resulting in a cost effective, high-performance answer to the challenges of 28 Gbps and beyond. Samtec Flyover™ QSFP28 Cable System Samtec proudly announces the release of the new Flyover™ QSFP28 … [Read more...]
Samtec and Molex Share High Speed Product IP
Our friends at Signal Integrity Journal recently reported Samtec's and Molex's collaboration on high speed, next-generation data centers. The complete article is worth the read, but here's the Cliff's Notes version: SIJ referred to the Licensed Source Agreement for the Samtec Twinax Flyover™ and Molex BiPass™ systems fo high-speed data (56 Gbps and 112 Gbps) speeds. According to a Molex spokesperson, both product lines approach their customers’ design challenges in the same … [Read more...]
Samtec Twinax Flyover QSFP-DD Cable Maintains SI Performance in Rugged Environments
Samtec recently completed an arduous flex and bend test on our Eye Speed® Ultra-Low Skew Twinax cable. This is used in our high speed cable assemblies, including the Samtec Flyover™ FQSFP-DD cable assembly. Besides achieving outstanding electrical performance, the testing has proved the cable to be rugged and provide stable electrical performance after repeated cycles. QSFP-DD 101 QSFP-DD is a new module and cage/connector system similar to current QSFP, but with an … [Read more...]
DINI Group Leverages Samtec FireFly™ for Low Latency HPC
Blockchain. Cryptocurrencies. Bitcoin mining. Algorithmic trading. These disruptive technologies depend on high-performance computing platforms for reliable execution. The financial services industry invests billions in hardware to support the near real-time services consumers require. Many financial services computing applications rely on x86-based server solutions. Alternative computing architectures leveraging the benefits of FPGAs are emerging. A combination of FPGA configurability, … [Read more...]
Samtec and Molex Collaborate on Next-Generation Twinax Data Center Solutions
Two global leaders in the design and manufacture of interconnects for high-performance electronic products today announced a Licensed Source Agreement (LSA) which brings together innovations that provide a new generation of solutions to meet the evolving needs of 56G and 112G data speeds. Samtec and Molex are the only suppliers licensed to offer the Samtec Twinax Flyover™ and Molex BiPass™ solutions. The combined solutions answer the needs of the growing number of high-speed applications … [Read more...]
Samtec Demonstrates 56 Gbps PAM4 QSFP-DD Cable Solution
56 Gbps, PAM4 System A new breed of cable solution is benefitting designers by reducing board size and improving signal performance -- either across the board, between boards, or from board-to-front panel. In this video, Ralph Page walks us through a combined Xilinx and Samtec 56 Gbps PAM4 FQSFP-DD to AcceleRate® cable demonstration. The QSFP-DD pluggable form factor, which supports 400 Gbps throughput – that is, 8 X 50 Gbps – is going to define front panel I/O on next generation … [Read more...]
112 Gbps PAM4 Micro Twinax Cable Demonstration
Credo, Samtec 112 Gpbs PAM4 Long Reach Over Cable Demonstration from Samtec on Vimeo. 112 Gbps PAM4 Keith Guetig, Samtec's High Speed Product Manager, walks us through a Credo + Samtec 112 Gbps PAM4 high-speed cable demonstration. This demo, showcasing Samtec's Flyover™ cable technology, was presented at OFC 2018 in San Diego, California. Signal Path and Equipment Two ports of 112 Gbps PAM4 data are sourced from the Credo CDRs. The signals route through RF jumpers to … [Read more...]
56/112 Gbps PAM4 Modular System Architecture With Samtec Flyover
Modular System Architecture Traditional communication and switch architecture leverages integrated designs in a single high-speed PCB, but this architecture is beginning to face signal integrity and thermal challenges at 56 and 112 Gbps PAM4. Samtec Flyover™ QSFP-DD solutions offer improved signal integrity and enable new modular system architectures, which also improve thermal efficiencies and lower costs. These next generation modular system architectures also enable greater design … [Read more...]
Key OFC 2018 Takeaways
There are few better places to be in March than San Diego. SoCal sunshine always beats wintry weather. Thankfully, OFC 2018 was located at the San Diego Convention Center instead of the snowy US East Coast. The sunny weather outside acted as a harbinger of the positive energy inside the convention center at OFC 2018. The technical sessions were filled with roadmaps from components and solutions providers. Attendees were eager with anticipation to see what the show would bring. Strong … [Read more...]
OFC 2018: Products, Technologies, Live Demonstrations
OFC 2018 OFC 2018, The Optical Fiber Communication Conference and Exhibition, is the largest global conference and exhibition for optical communications and networking possibilities. Next-generation optical communication and networking applications must solve multiple technical challenges including higher data rates, increased system and chassis density, and improved signal integrity. Samtec’s diverse product and technology portfolio, which provide system designers with architectural … [Read more...]
- « Previous Page
- 1
- …
- 10
- 11
- 12
- 13
- 14
- …
- 17
- Next Page »