For many patients, their care does not end when they leave the hospital. Therapeutic equipment is used when the patient needs long-term assistance or care. The many uses for electronics in therapeutic equipment require a range of interconnect solutions that combine power and data. Prosthetic Devices The use of artificial or prosthetic limbs or is not new, although global events of the last two decades has brought them more into the public eye. With advances in emergency medical care, the … [Read more...]
Sudden Service is Essential for Essential Industries
Sudden Service is the foundation of Samtec. This core part of our DNA is what has prepared us to react to the chaos that has continued to hit essential industries across the globe. Supply chain issues, material cost increases, and chip shortages are just a few things we struggle with daily alongside many of you. How do we react, how do we keep our customers working in essential industries going? Read along as we explain a bit about how we operate and support you as a long running customer or as … [Read more...]
New Connector Search Gives You A Mated Connector Set In Seconds
A Good Problem? Samtec has more ways to stack two or more boards together than any other connector company. Our manufacturing process allows us to position the plastic body on the terminal pin in increments of .005” (0.13 mm) on standard dual-body stacking connectors and on standard terminal strips (“headers”). Designers can create standard part numbers for very precise, non-industry-standard-board stacking heights. The good news is we have literally millions of connector … [Read more...]
A Student’s Perspective – Smart Cities, Smart Grids and Smart Factories
Smart cities, grids and factories are exciting and rapidly innovative industries in today’s world. As an Electrical Engineering student at San José State University in the heart of Silicon Valley, I can observe the innovation real-time. For example, the city of San José seeks to be the "smartest" city on the planet. As I progress in my studies, I look forward to seeing the practical applications in Smart Cities efforts. Smart Cities - What are they? A smart city is a framework to … [Read more...]
Medical Vision Systems
In order to provide medical care, it is important to understand what is happening inside a patient’s body. The latest generation of vision systems is allowing doctors to create accurate imaging. This is providing a new understanding of the human body and is enabling a whole new approach to surgery and medical care. One of the key reasons that imaging is so important in successful diagnosis and treatment is that every patient is different. Each patient has a unique anatomy, and each will … [Read more...]
New SMPM Precision RF Cable and Board Level Connectors
Precision RF Connector Systems Samtec continues to expand its line of precision RF cable-to-board and board level connectors. We offer a full line of off-the-shelf products for microwave and millimeter wave applications from 18 GHz to 110 GHz. Precision RF products support next generation technology advancements in wireless communication, automotive, radar, SATCOM, aerospace, defense, and test and measurement. SMPM Products Samtec now offers a full line of SMPM solutions with a maximum … [Read more...]
Ask The Expert – Precision RF Connectors
We live in an age of digital technology, but it is easy to forget the importance of radio frequency (RF) transmission. Any device that transmits or receives its signals uses RF radiation to carry data. The physical infrastructure needed to transmit radio frequency signals uses coaxial cables and connectors. These RF connectors and cables need to transmit the highest signal speeds and introduce the lowest possible losses for data to reach its destination safely. The latest precision RF … [Read more...]
New High Speed Cable System Enables 112 Gbps PAM4
A new high speed cable system, which enables 112 Gbps PAM4 signaling, can be used in mid-board, mid-board-to-front-panel, and panel-to-panel applications. This video from DesignCon 2021 shows a live product demonstration with a Samtec NovaRay®, Flyover® Cable system operating at 112 Gbps PAM4, as well as a Bulls Eye® high-performance test cable system. It’s all driven by a Xilinx ® Versal™ Premium GTM transceiver. The Versal Premium ACAP allows vendors to position their … [Read more...]
Connectors for Patient Care Applications
The needs of the medical profession to provide patient care go beyond the safe conditions of the operating room and the hospital. Many patients are cared for in other environments – doctors’ offices, health centers and increasingly, in the home. This is especially true for patients who require long-term care, and the technology that they need faces the challenge of being used far from the confines of the hospital. This is not a new trend. For many years, healthcare professionals have made … [Read more...]
New High Data Rate 112 Gbps PAM4 Connector System
System architects and design engineers are interested in bleeding-edge performance. In this new 112 Gbps PAM4 product demonstration, Samtec marries an SI Evaluation Kit for the new AcceleRate®HP interconnect system with a Synopsys 112 Gbps PAM4 transceiver test chip. AcceleRate® HP is one of several Samtec connector systems rated at 112 Gbps PAM4, and it also provides outstanding design flexibility. The test set-up emulates real-world, high data rate applications by routing differential … [Read more...]
- « Previous Page
- 1
- …
- 25
- 26
- 27
- 28
- 29
- …
- 62
- Next Page »