The gang’s all here! We’ve recently pulled together Samtec’s family of AcceleRate® products into one webpage so you can easily browse and compare to find the best high-performance solution for your next gen application. The board-to-board and cable assemblies feature extreme density with up to 1,000 total I/Os on a 0.635 mm pitch and extreme 112 Gbps PAM4 performance. So, let’s get this party started with (re)introductions all around… Board-to-Board Interconnects First up is … [Read more...]
Samtec.com Continues to Speed up Through Use of Static Website Technology
In the last several months of website updates, we've sprinkled in some tidbits about our static website conversion project. This project entails converting many areas of the Samtec.com website from being served from web server storage and sometimes slower database lookups to serving them straight from the web server cache. Caching works by taking advantage of the benefits of RAM to significantly increase the speed at which a webpage can be delivered to a user. Because this technology is … [Read more...]
Embedded World 2022: Samtec Connects a Smarter World
COVID-19 is slowly fading away. People are returning to a normal life. Students look forward to summer. Families are planning holidays. Friends and colleagues are sharing meals in restaurants. In the business world, virtual meetings are still a reality. Yet, many professionals yearn to see their colleagues in person. Slowly but surely, in-person connections are being made via trade shows. Next week in Nuremburg, the annual embedded world event returns. The Coronavirus Omicron variant … [Read more...]
IMS 2022: New Technology, Millimeter Wave Connectors, and RF Launches
IMS 2022 is a week dedicated to all things microwave and RF. It’s the premier event where thousands of RF and microwave professionals will gather this June for networking, education, and to visit the exhibition. Samtec is looking forward to presenting our newest microwave / millimeter wave connector products, as well as showcasing some new technologies and applications in five live demonstrations and static displays. Microwave, Millimeter Wave Products Samtec designs and manufactures … [Read more...]
Connectors for Data Acquisition
Data is the raw material of the future. The advent of the Internet of Things has transformed many activities in the modern world, from growing the food we eat to the way our healthcare is provided. Enabled by the increased capabilities of modern processors and the speed of the latest communication, data will become just as important as steel and energy. The Internet of Things is allowing machines to share information with each other for the first time. In just one example, machines in the … [Read more...]
New 1.35 mm Precision RF Products to 90 GHz
Samtec has released its 1.35 mm family of products suitable for millimeter wave applications to 90 GHz. The 1.35 mm family includes compression mount board connectors (135 Series), cable connectors (PRF13 Series) and .047" low-loss flexible cable assemblies (RF047-A Series). 1.35 mm products are ideal for IEEE, E-band applications due to their high operating frequency and electrical precision. Samtec’s 1.35 mm board connectors are the industry’s only vertical compression mount product using … [Read more...]
Next-Gen Blue UAS Framework 2.0 AutoPilot Features Samtec High-Speed Interconnect
UAVs, or drones, have been around for decades. Original drones resembled early generation fighter jets controlled from the ground and used as targets for test pilots. As time passed, drones served as high-tech reconnaissance platforms and high-precision offensive weapons in military applications In recent years, drones have found many commercial uses as well. Popular e-commerce platforms and global retailers are using drones for order delivery. Hobbyists and tourists use … [Read more...]
Do You Want to Go Fast?
With the global headquarters of Samtec in Southern Indiana, we are surrounded by people wanting to go Fast! A few weeks ago we watched horses go fast in the 148th Kentucky Derby. This past weekend we watched Indy Cars go fast during the 106th Indianapolis 500. A driver or jocky's decision-making and reaction time made me think of delays or latency when it comes to the interconnect market. High-speed connectors are a sweet spot for Samtec and if you are unfamiliar with some of our offerings … [Read more...]
Wideband RF Launches: Literally, Everything You Need To Know
As the demand for higher frequencies and wider bandwidths continue their relentless march upward, RF connectors need to keep up and even exceed this demand. Mating the RF connector to a PCB or substrate requires careful consideration of several factors to get the full performance out of the connector. Let’s frame this concept by starting with a simple analogy: Putting tractor tires on a race car is not a recipe for success. Tires on a race car need to convert power from the engine … [Read more...]
Optics in VPX with VITA 66
VITA 66 has been around for some years now. What goes into this standard continues to expand. VITA 66 is an evolution to increase your options inside the existing VITA 46 (VPX) market space. Samtec is pleased to announce the addition of our VITA 66 Landing Page. We are designed in VPX applications around the world! (Both on the ground and in space!) This page is dedicated to helping you find the right mid-board optics connectivity options more efficiantly. VITA 66.0 is the base … [Read more...]
- « Previous Page
- 1
- …
- 18
- 19
- 20
- 21
- 22
- …
- 62
- Next Page »