As the demand for higher frequencies and wider bandwidths continue their relentless march upward, RF connectors need to keep up and even exceed this demand. Mating the RF connector to a PCB or substrate requires careful consideration of several factors to get the full performance out of the connector. Let’s frame this concept by starting with a simple analogy: Putting tractor tires on a race car is not a recipe for success. Tires on a race car need to convert power from the engine … [Read more...]
A Performance Comparison of Air-Cooled vs. Immersion Cooled Connector Systems
As computing power continues to increase, air cooled systems cannot meet current thermal requirements for HPC hardware systems. Power consumption, space and performance must all be considered during system design. Immersion cooling is a fast-growing solution to economically combat system heat, noise, power consumption and compute density. Samtec’s Brian Niehoff presented “Thermal Management of HPC Hardware Architecture via Immersion Cooling” at the Exhibitor Forum at SC20. Brian’s … [Read more...]
Solder Processing with Success
Processing a component onto a PCB used to be fairly straightforward. Through-hole products, or a single or double row surface mount with a larger centerline rarely offer unique challenges obtaining a proper solder joint. However, as electronics continue to get smaller and connectors become more dense, there is a need to ensure that the inner rows of the connectors properly solder and obtain a strong solder joint. Connector manufacturers have addressed this in many ways, and one of the ways … [Read more...]
Selecting The Right Connector, Part 2
In Part 1 of this blog, I introduced you to Mr. Phil Eckert, Samtec's Quality Engineering Manager. Phil shared seven tips to help designers select the right connector system for their application, and to generally make your life easier. Today, in Part 2, Phil gives us eight more tips to help you choose the right connector system for your design. 1. Flux: Unspent flux is problematic in connectors from both a mechanical interference and a corrosive nature. Ultimately this can result in … [Read more...]
Selecting the Right Connector, Part 1
Inventing the light bulb, phonograph, motion picture technologies, film, the mimeograph, and holding a record 1,093 patents is impressive. But, I bet Thomas Edison never had the truly difficult job of selecting the right connector system for his printed circuit boards (PCB), nor did he have to work with process or quality engineers to make sure said connector systems were designed-for-manufacturability. That's where Phil Eckert comes in. Phil is Samtec’s Customer Quality Engineering Manager … [Read more...]
Challenges Of Aligning Multiple Connector Sets
Increased density, shrinking footprints, higher data rates, and thermal management are but a few of the challenges affecting the design and fabrication of printed circuit boards (PCBs) in today’s electronic systems. And did I mention cost? An important, although sometimes overlooked consideration, is these increasingly sophisticated PCBs often require more complex connector systems. Most of the aforementioned design factors also affect connector design and performance, including smaller … [Read more...]
Understanding IPC Class 2 vs Class 3 for a Gull Wing Lead
IPC-A-610 covers a wide range of solder joints, and what it takes to meet Classes 1 - 3 in varying types of connector termination styles. These classifications help a designer determine if a connector is capable of being used in their application. In a previous blog, I discussed IPC Class 2 vs Class 3 solder joints for J-Lead Components, and in this one we will look at the difference for Gull Wing Leads. In case you were wondering, a gull wing lead is a type of surface mount lead that is … [Read more...]
Understanding IPC Class 2 vs Class 3 Solder Joints
In the manufacturing world there are standards for just about everything, and they all are typically there to ensure a product can perform as expected for the end application. Among these standards is IPC-A-610 covering solder joints for varying types of connector termination styles. For this blog, we are going to take a quick look at IPC-A-610 Class 2 and Class 3 solder joints, and some of the requirements of those two classifications. To narrow the focus further, we are looking at a J-Lead … [Read more...]
The Effects Of Lubrication On Connector Processing
Decisions, Decisions ... I may be in the market for a new car in the near future. Unless you’ve got a strong preference (and most car buyers DO have a strong preference, IMO), choosing a vehicle is a series of trade-offs. Fuel efficiency vs. horsepower. Functionality vs. appearance. Safety vs. fun. Cost vs. a heated steering wheel and seats. Choosing the right connector set for many EOEM applications is also full of trade-offs, including pitch, termination type, plating, and contact … [Read more...]
Connector Thermal Cycle Qualification For Military and Avionic Environments
Collins Aerospace recently published a white paper entitled “Qualification Of High Density Connector Solutions For Military and Avionic Environments.” It discusses their qualification process of high density connectors for rugged military and avionics applications. This paper focuses on the thermal testing of solder joints because “printed circuit board (PCB) assemblies are made up of many different materials that have different coefficient of thermal expansion (CTE) … [Read more...]