Advanced Technologies Augment Samtec Technology Roadmap for 3-D Packaging, Sensor Modules, and Wireless Connectivity New Albany, IN, May 31, 2016 – Samtec, Inc., a leading provider of high bandwidth and micro-pitch interconnect systems, announced today the acquisition of nMode Solutions, of Oro Valley, Arizona. “The acquisitions of nMode Solutions and their subsidiary, Triton Microtechnologies, is a critical next step in Samtec’s technology roadmap. This furthers our … [Read more...]
Xilinx and Samtec Deepen Technical Collaboration
Higher data rates in today’s bleeding edge ICs require constant innovation in interconnect to route signals on PCBS and between them. Samtec’s Silicon to Silicon System Optimization provides engineers the service, products, tools and resources to optimize the entire signal path from bare die to IC package and assembly to PCB to connectors and cable assemblies and back again. A practical case study in our Silicon to Silicon System Optimization capabilities is leading FPGA vendor Xilinx. … [Read more...]
Samtec Releases Micro Discrete Wire Application Design Guide
Wire-to-board connectors have been around for decades. They evolved as a solution for easier manufacturing in modern electronics versus legacy terminations such as soldering wires directly to the board. Standard .100” (2.54mm) pitch wire-to-board socket and headers can be found in many industrial and transportation applications for both signaling and power. The PC revolution on the 1980s and 1990s pioneered IDC systems linking hard drives, power suppliers and other I/O devices … [Read more...]
Eric Bogatin’s Three Predictions On The State Of Signal Integrity
Signal Integrity expert Eric Bogatin recently shared three predictions on the state of signal integrity. Based on his discussions at DesignCon 2016 and thereafter, Eric has three predictions about major changes ahead for high speed serial link systems. The first is the rollout of 28 Gbps systems will be slower than expected. Eric explains that the semiconductor companies producing the CMOS devices – ASIC, FPGA or custom – are doing fine producing the silicon with acceptable performance at 28 … [Read more...]
Avnet Industrial IoT Starter Kit Includes Samtec
No matter where we look the amount of devices connected to the Internet continues to grow. It seems but only a few years ago that a PC with a dial-up 56 kbps modem was bleeding edge. Households with internet connectivity measured in the millions. According to one source, only 1% of the world’s population had Internet connectivity in 1995. Obviously, times haves changed with smart phones, wearable fitness devices, media players and other commonplace Internet-connected consumer … [Read more...]
Samtec Releases Twinax Flyover Application Design Guide
The march to faster data rates never seems to stop. Communications protocols used in the data center provide the proof. Fiber Channel signals can run up to 32 Gbps. 25G Ethernet 802.3bj and Ethernet 100G signals can run up to 25Gbps. InfiniBand EDR 104G serial channels support 26 Gbps data rates. This presents engineers of high-speed serial channels with a number of PCB design challenges. Some of the key limitations of PCBs running at 28+ Gbps include trace … [Read more...]
Samtec Updates Broadcast Video Solution Guide
Streaming HD video and 4K/8K UHDTV are just two examples of a continuing evolution in video signaling. Video has transformed from being an analog 6 MHz bandwidth signal to a 12 Gbps digital data stream. As signaling has transitioned into the digital domain, first in SD and HD formats, and recently at 6 Gbps and 12 Gbps 4K UHD-SDI standards, the demand for meeting stringent return loss requirements up to 12 GHz has emerged. Samtec offers a full line of high-speed board-to-board and RF … [Read more...]
High Speed Signal Transfer Rates At 28 Gbps (OFC 2016)
In this video, Kevin Burt, of the Samtec Optical Group, discusses another demonstration from OFC 2016. This is a system level demonstration of high speed signal transfer rates at 28Gbps, FireFly™ high speed optical links at 28 Gbps, and signal quality performance of ExaMAX® backplane connector. Kevin discusses the advantages of the industry's first Flyover QSFP28 (FQSFP) System. This approach removes signals from their traditional pathways—copper traces … [Read more...]
14 Gbps Optical Link In FMC VITA 57.1 Form Factor For FPGA Applications (OFC 2016)
Kevin Burt, of the Samtec Optical Group, discusses one of two demonstrations at OFC 2016. This is a demo of a FireFly™ 14 Gbps optical link in a FMC VITA 57.1 form factor for FPGA applications, for the high performance computing, rugged military, and industrial markets, to name a few. This demo is an optical interconnection between two FPGAs, with a Xilinx Development Card and two FMCs (FPGA mezzanine cards), one from TechWay and the other from Crossfield Technology. This is 8 lanes of 14 … [Read more...]
Samtec Exhibits at 2016 NAB Show in Las Vegas
One of the biggest tradeshows in entertainment and media is NAB Show. It is the world’s largest annual conference and expo for professionals who create, manage, and distribute entertainment across all platforms At this year’s event in Las Vegas, Samtec will feature a variety of interconnect solutions targeted at the broadcast video market. These include mid-board and panel mount optical systems based on FireFly™ , True75TM 75Ω RF Systems, full turnkey RF cable assemblies, and … [Read more...]
- « Previous Page
- 1
- …
- 36
- 37
- 38
- 39
- 40
- …
- 42
- Next Page »