The global XDF technology road shows come to Beijing next week. FPGA designers, system architects, data scientists and other technical leaders will gather December 3-4, 2019 at the China National Convention Center. Samtec technical experts and our partners will demonstrate some of the latest interconnect solutions affecting the Xilinx FPGA ecosystem. Samtec Interconnect on Xilinx Kits One of several demonstrations at XDF 2019 Asia shows the variety of Samtec interconnects supporting … [Read more...]
Search Results for: VITA 57
AI, 5G and Automotive – Dispatches from XDF Silicon Valley
The FPGA (or ACAP) universe gathered at the San Jose Fairmount last week during the Xilinx Developer Forum. Engineers, data scientists, analysts, distributors, alliance partners and more came to learn about the latest hardware, software and system level solutions from Xilinx. Xilinx CEO Victor Peng set the theme of the event with his keynote. Xilinx (and thier partner's) business strategies revolve around three key growth drivers: Data Center, 5G and Automotive. The Samtec team … [Read more...]
New Intel FPGA Platform Features Samtec Interconnect
Transceivers. SerDes. XCVRs. Tx/Rx. Yada, Yada, Yada. FPGA designers want more of them. FPGA designers want them to be faster. Thankfully, the leading FPGA suppliers are answering the call. The Samtec blog features many solutions from Xilinx, but what about Intel? What options are they promoting? Intel® Agilex™ FPGA and SoCs Intel recently released their latest FPGA/SoC platform called Intel® Agilex™. This family leverages Intel's 10nm process technology and advanced architectures. … [Read more...]
Don’t Forget Bulls Eye® and FPGAs on Vacation
Prime vacation (or holiday) season is in full gear. Travel spots range from the beach to cultural attractions in the latest "hot spots". Whether sunning in the Côte d'Azur or hiking in the Andes, everybody's focus is their . . . smart phone? Really? For (almost) everybody, the latest moment MUST be shared on social media. What happens when no connection is available? Panic! Fortunately, connectivity is almost everywhere. Just ask the closest teenager! What does this have to do with … [Read more...]
New Optical FMC+ Module Supports Extended Temperature Ranges
Readers of the Samtec blog are familiar with the benefits of FMC and FMC+. These popular interfaces define a compact electro-mechanical expansion interface for a daughter card to an FPGA baseboard or other device with re-configurable I/O capability. VITA 57.1 has been around for some time. It supports 10 full-duplex transceivers running at 10 Gbps. The new VITA 57.4 standard defines two new connectors. Combined, they offer 32 full-duplex transceivers running at 28 Gbps. New … [Read more...]
New Zynq UltraScale+ Platform Offers 32 Gbps via FMC+ and FireFly™ Interfaces
One of the most popular interfaces in the FPGA world is FMC. This has recently been expanded to FMC+. The new VITA 57.4 standard defines two new connectors. Combined, they offer 32 full-duplex channels running at 28 Gbps. However, the current generation of FPGAs and MPSoCs have transceivers supporting data rates in excess of 32 Gbps. Why? Emerging protocols – including PCIe Gen 5 and JESD204C – will run at 32 Gbps. Engineers developing solutions using 32Gbps+ protocols need … [Read more...]
Samtec Website Updates for 2018 – A Year in Review
Wow! How quickly the web evolves. Just a few years ago we were building a new version of our website from scratch using a completely new codebase. Since then, we've done hundreds of releases to stay current with web technology and user expectations, and I'm sure we will do hundreds more. As the expectations of web users in the B2B space continue to evolve rapidly, 2019 will be no different, and will pick up even more steam. But before we look too far ahead to what's in store for … [Read more...]
Evaluation and Development Kits Viewable Across Samtec.com
Over the past few years, Samtec has expanded its portfolio of Evaluation and Development Kits. Engineers and designers demand the best tools for system prototyping. From concept and prototype to development and production, Samtec-designed Evaluation and Development Kits featuring high-speed interconnect solutions to help simplify design. Helpfully, they reduce time to market for hobbyists, tinkerers, start-ups and OEMs alike. Easy Access via Landing Page Engineers want instant access … [Read more...]
High Speed Interconnect Demos At Electronica 2018
Samtec's full line of high speed interconnect products was on display and in demonstrations at Electronica 2018. Focus products included high speed mezzaninehigh speed cable assemblieshigh speed backplane connectorsactive optical cable assemblies Two of the demos that caught a lot of attention were the 28 G Product Demonstrator and the REFLEX CES Sargon Stratix 10 FPGA FMC+ IDK. 28 G Product Demonstrator In this video, Samtec's Neil Potter walks us through the 28 G … [Read more...]
Samtec Features Latest High-Performance Copper and Optical Solutions at SC18
Next-generation high-performance copper and optical interconnects must solve multiple technical challenges including higher data rates, increased system and chassis density, and improved signal integrity. Samtec’s diverse product and technology portfolio provides system designers architectural solutions to the challenges faced by the industry. Several key solutions will be featured at SC18. SC18 Demonstrations Samtec and its partners feature an extensive number of demos at SC18. A … [Read more...]
- « Previous Page
- 1
- 2
- 3
- 4
- 5
- 6
- …
- 9
- Next Page »